El último modelo de RPi no tiene el enganche a Bayoneta para la SD.
Sólo funciona con SD de 16 gigas o se pueden utilizar de 8 gigas?
El último modelo de RPi no tiene el enganche a Bayoneta para la SD.
Sólo funciona con SD de 16 gigas o se pueden utilizar de 8 gigas?
Hi all.
Thank you for your reply.
The RPI until the version 2 had a locking system for the sd who also served as ejection system.
RPI 3 does not have this system?
Can I use the RPI with a Sd 8GB?
I tried to move the file from the SD 16GB to the 8GB one, but the system will not start.
Best regards.
Vittorio
The size of the sd card needs to be big enough for the o/s you pick. I used 8GB for a fresh download of Rasbian Jessi full edition which was dated Feb 29, 2016 and the Pi 3 worked fine. Older version may not work unless properly updated with 3 commands.
Clem
The size of the sd card needs to be big enough for the o/s you pick. I used 8GB for a fresh download of Rasbian Jessi full edition which was dated Feb 29, 2016 and the Pi 3 worked fine. Older version may not work unless properly updated with 3 commands.
Clem