Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi3 B+ to 8 channel relay CODING HELP
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 3 answers
  • Subscribers 706 subscribers
  • Views 2468 views
  • Users 0 members are here
  • 8 channel relay
  • home automation
  • automated
  • raspberry_pi
  • pi3
  • rasberry pi 3
Related

Pi3 B+ to 8 channel relay CODING HELP

e14 Contributor
e14 Contributor over 10 years ago

Hello, I will be blunt and honest, This is my first time looking at a Linux system let alone trying to learn to code in python and I'm struggling big time trying to learn this all. I need a coding mentor who is willing to communicate with me and help me get this done. Ahead of time, I apologize for my lack of vocabulary and my unorthodox techniques and perspective and thank you for your everlasting patients and I really appreciate any and all time you invest into helping me!

 

Question: Will you look over my project (posted below) and help me get it coded? ideally, i would be able to have an interface that would allow ease of use programmable on//off cycle on each outlet (all 8) and also in addition to, a simple toggle on//off of all 8 as well.    ( example:    [OUTLET 1]  on=15 minutes   off=45 minutes * repeat*

                                                                                                                 [OUTLET 2]  on= 16 minutes   off=44 minutes *repeat*

                                                                                                                 [OUTLET 3]       on=2pm         off=11pm

                                                                                                                 [OUTLET 4]      ON

                                                                                                                 etc....etc......)

Here's where i am so far the best i can sum it up;

Pi3

Relay       Diagram of relay

CanaKit GPIO to Breadboard Interface Board

 

This is how i wired the relay to the main power source

 

 

image

 

Below is a how I wired the breadboard to the relay. (Picture is visual rep of it written out)

 

Relay       |      Gpio# 

JD=Vcc            5v                                           

GND                GND

 

Vcc                  5v

1n1                GPIO 17

1n2                GPIO 27

1n3               GPIO 22

1n4               GPIO 23

1n5              GPIO 24

1n6              GPIO 26

1n7              GPIO 12

1n8              GPIO 16

 


image

what do you think? Can you tailor some code for me? I'm sure the code is out there some where, I most likely just need some guidance on how to fine tune it to my wiring/setup. 

 

                                                  Anxiously and hopefully awaiting a response 

                                                                      ~Mathew

 

 

 

 

* WORKING WITH ELECTRICITY IS EXTREMELY DANGEROUS. DO NOT TRY THIS. THIS IS A HYPOTHETICAL PROJECT NOT MEANT TO BE DUPLICATED OR REPRODUCED BUT FOR EDUCATION PURPOSES ONLY. ALWAYS USE ALL SAFETY STANDARDS WHEN WORKING WITH ELECTRICITY PER YOUR AREAS LAWS AND REGULATIONS*

 

Message was edited by: Mathew Rawlings THANKS PETER

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    Logically, everything looks good.

     

    Electrically ti are not following safe standards and while it is up to you if you do this on your projects, you need to consider that others will follow your example

     

    The relay board should be in a safe housing. It has mains on it and as such should be correctly protected from people sticking their fingers into it.

    Using standard and approved power outlets is a good thing, especially if they are in the approved enclosure and with the right covers in place.

     

    You need to add words of wisdom indicating to viewers that if they are not familiar with working with mains then they should get help from someone that is., add the fact that not doing this can lead to death or worse.

     

    You need to add that Electrical Code is different for each country and province so people should be aware and follow their local codes of practice or dont do this.

     

    Hope this helps

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    Logically, everything looks good.

     

    Electrically ti are not following safe standards and while it is up to you if you do this on your projects, you need to consider that others will follow your example

     

    The relay board should be in a safe housing. It has mains on it and as such should be correctly protected from people sticking their fingers into it.

    Using standard and approved power outlets is a good thing, especially if they are in the approved enclosure and with the right covers in place.

     

    You need to add words of wisdom indicating to viewers that if they are not familiar with working with mains then they should get help from someone that is., add the fact that not doing this can lead to death or worse.

     

    You need to add that Electrical Code is different for each country and province so people should be aware and follow their local codes of practice or dont do this.

     

    Hope this helps

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer