Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi3 Does not boot up - Green light does not lit
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 34 replies
  • Answers 4 answers
  • Subscribers 719 subscribers
  • Views 9300 views
  • Users 0 members are here
  • pi3 does not boot up
Related

Raspberry Pi3 Does not boot up - Green light does not lit

e14 Contributor
e14 Contributor over 10 years ago

I purchased a Raspberry Pi3 last week, after spending couple of days trying to get it to boot up I gave up and purchase another one. I am having the same issues, it just would not boot up, i.e. the green light does not lit -- which I think means that is Not reading the SD card to load the Operating System. This is what I have done so far:

Used a 5v/2A power supply, use a 5v/2.4A power supply.

Used the SD with the preloaded OS that I purchased - no luck

Purchase another SD card, formatted it and load Noobs sw on it - still no luck

I removed every thing that is plugged in the PI3 except for the power supply, still no luck.

 

Anyone out there who is experiencing the same issue???

Does your one works out of the box?

 

What am i doing wrong???

 

What should the voltage/Amp for the power supply be? is it 5v/2.5A?

Help please.. Gerard

  • Sign in to reply
  • Cancel
  • shabaz
    0 shabaz over 8 years ago in reply to ennemm

    The on-the-street hearsay is that >90% of any returns are user error, and not faulty Pi's. There isn't enough detail to conclude that the Pi is defective.

    Some more information would be needed, specifically what power supply and cable are you using? What else is attached? And is there a photo showing the insertion of the micro SD card, if there is any doubt from you that it may not be pushed/seated correctly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ennemm
    0 ennemm over 8 years ago in reply to shabaz

    Thanks for responding. I will get more details to you esp power supply and photo,  as soon as I can get to the device at home.

     

    Meanwhile, as mentioned, same (recently full formatted new NOOBS/Raspbian) SD card when used with same setup (USB cables, power cable) inserted in identical way but into my RPi 2 works just fine. RPi 3 shows no green light any time.  Only power supply and monitor USB plugged in.  With or without keyboard and mouse same result.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ennemm
    0 ennemm over 8 years ago in reply to ennemm

    Solved.  Went to Microcenter, bought a new identical RPi 3, bought a recommended power supply. Put the same SD card in and all worked. Then swapped just the problematic RPi 3 and only red light. So concluded faulty unit and showed and informed them, they swapped it!  The new R Pi 3 works fine even with my regular 2v phone charger.

     

    So I got the rare bad apple. Should have done this sooner.

     

    But thanks all for the suggestions and to OP for this thread.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 8 years ago in reply to ennemm

    Great, glad it is solved! Many other supplies are borderline, because the Pi spec is slightly different to what USB standard specifies, so the 3A supply is 'special' in that it has thicker wires than normal, and possibly quite tight specification on the voltage output. But other supplies and USB cables can work, just sometimes hard to know for sure unless it is tried.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • thehwcave
    0 thehwcave over 8 years ago

    Hi Gerad,

    couple of things I would try and see where it leads you.

    First: (silly question) the SD card is the right way around and all the way in?

     

    Second: the power supply (2A is plenty): use it to plug into a mobile phone or tablet (or anything with a micro USB) and see see if it gets power.

     

    Third: plug the power supply into your RPI (and nothing else in case some of your peripherals have a problem). Use a multi-meter between the GPIO pins for +5V and GND and check if you see 5V. If you do, also check the +3.3V pin.

     

    Can you let us know what the result is?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • thehwcave
    0 thehwcave over 8 years ago in reply to thehwcave

    In case you don't know the pin-out of the GPIO can be found here:

     

    https://www.raspberrypi.org/documentation/usage/gpio-plus-and-raspi2/README.md

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dxslim
    0 dxslim over 8 years ago in reply to shabaz

    I have almost 100 boards in service. Of those 100, I had three out-of-box failures: 1 mechanical-intermittent, 1 rainbow-screen-of-death, and 1 does-not-a-damn-thing. I had my tech reflow all three on the chance that the failures are all due to bad solder. The mechanical-intermittent "recovered" but the other two are still scrap. The Pi is a wonderful product, but 3% failure on boards that have passed factory test is kinda dismal quality.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • marsierose
    0 marsierose over 7 years ago

    I was having the same issue today, i found instead of dragging and dropping into the sd card i had installed it in a folder i labeled noobs, which was the problem.. Thank you and I hope this is useful if anyone else has had this issue

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • agnessa1
    0 agnessa1 over 7 years ago

    You should make sure the SD card is properly seated and formatted/installed correctly. And that you didn’t do anything to the board, because last time I tried, I accidentally broke a resistor thing for the CPU and totally trashed the board (it made the green light not work)

    No green means that no boot code was executed, so its probably having an issue reading it.

    What to do:

     

    Make sure card is seated property.

    Make sure your sd card/pi image has “bootcode.bin”, “fixup.dat”, and “start.elf”. And that you can read it.

    Make sure the SD card isnt damaged.

    Ensure the board isn’t damaged.

    Ensure the power supply is sufficient. The Pi 3 takes 5v and draws around 2 amps of current (Estimate is high but 1A isn’t good enough)

     

    Flash patterns:

    2 flashes: card couldn’t be read

    3 flashes: start.elf not found

    4 flashes: start.elf not launched

    7 flashes: kernel.img not found

    8 flashes: SDRAM not recognised.

    SDCard tools for formatting/installing Raspbian:

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • lyubcho
    0 lyubcho over 7 years ago

    I think there is a hardware issue mainly on this module and model b+ the only way is to get a new one from the place where you bought it hopefully you still have warranty. Hopefully I helped you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<>