Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum bcm2835_gpio_eds_multi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 705 subscribers
  • Views 681 views
  • Users 0 members are here
  • rpi3
  • rpi3b
  • raspberry_pi_space
  • rpi
  • bcm2835
Related

bcm2835_gpio_eds_multi

e14 Contributor
e14 Contributor over 10 years ago

Hello!  I trying to use the bcm2835_gpio_eds_multi() function to detect an low-level change on five inputs in a high-speed loop. Yes. I have init the ports with fsel(), pud() and len() functions earlier.

This eds_multi() just returning zero. Do I miss something?  The bcm-header talked about some "Device tree"...I have activated it (I don't know what that doing...).'

 

The code is

 

#define INT_PINS (1<<portA | 1<<portB | 1<<portC | 1<<portD | 1<<portE)

while(1)

{

     if( ret = bcm2835_gpio_eds_multi(INT_PINS)

     {

     printf("%08x", ret);

     bcm2835_gpio_set_eds_multi( INT_PINS );

     }

}

 

This "ret" should return something if I take the pin LOW.

 

I see one thing. Should the #define include a cast to a unsigned long int? I think so...

 

I would appreciate a hint...

(If it seems ok, I think it is the hardware...it's new)

 

Rgds

Swedland

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    I reply myself.  It was the CAN-controllers that didn't ACK the Interrupt. The INT-ports went low (correct) but never went high again. It was seen with a oscilloskope.
    I got the HEX-value from each of the INT-pins with the eds_multi() function and then chose the correct CS and trough the SPI put the correct INT-flag low.

    So, problem solved.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer