Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Power supply
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 703 subscribers
  • Views 637 views
  • Users 0 members are here
  • raspberry_pi
Related

Power supply

c_p
c_p over 10 years ago

Hi,

I have a display board which has a USB socket so I can power my raspberry pi. The display claims to need 3-4A but seemed to work fine with 2A when I tried with an adapter I had. I was also intending to power an rgb led strip with the same power supply (the 2A adapter was from this kit). I think I may be ok with a 6A supply but probably look at 8A to be sure. As the display and lights may be on or off, would I then require a regulated power supply such as this one:

http://www.ebay.co.uk/itm/182199432850

 

Or would I be better using something like this:

http://www.ebay.co.uk/itm/300916270368

 

I think I found somewhere which suggested that a dummy load would be needed for using a regulated power supply, would I need one in this case?

Thanks

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 10 years ago

    Hi c_p,

     

    I wouldn't trust any mains power supply like that, that cost just a few £. There's no short route to this, better to just use a known supply brick if you can find one around the home or buy one from a traceable source, e.g. farnell.co.uk, and it will come with a spec sheet with all the details - it won't be near this price however.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • c_p
    0 c_p over 10 years ago in reply to shabaz

    Thanks, thought I had seen a couple of geniune CE marks rather than the fake ones but after seeing the prices on farnell I doubt they're trustworthy. Found this one  which seems like it could be reasonable and the datasheet says I don't need any minimum load so I'm happier about using it

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • c_p
    0 c_p over 10 years ago in reply to shabaz

    Thanks, thought I had seen a couple of geniune CE marks rather than the fake ones but after seeing the prices on farnell I doubt they're trustworthy. Found this one  which seems like it could be reasonable and the datasheet says I don't need any minimum load so I'm happier about using it