Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum NesPi Needs More Power
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 26 replies
  • Answers 3 answers
  • Subscribers 709 subscribers
  • Views 4797 views
  • Users 0 members are here
  • nespi power
  • raspberry_pi
Related

NesPi Needs More Power

e14 Contributor
e14 Contributor over 10 years ago

So i am doing the nespi project and have found that i need power to a usb hub and power to the pi. I only have installed one usb 3.0 port for power to come into the nes case. If i get this power supply --> https://www.amazon.com/Adapter-Portable ... wer+supply

 

Can i take two usb cables from ^^^this power supply from a usb splitter into a single usb cable then split it back out into two usb connections. Then have one end go to the pi and the other end go to the usb hub to power both devices.

 

Another possibility i have thought of is trying to bring more amps to the usb hub but i do not know it it can handle more power in and if that would allow it to output more power per port.

 

I would also greatly appreciate any other ideas on how to get power to both devices with only using one usb port to get power into the case.

 

Attached is the setup before the powered usb hub was added in to power the 4 controllers separate from the pi's power. And the back port is the single usb 3.0 port i have to bring power into the case.

 

Hopefully later i can get a pic of that to help with any questions on the setup.

Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    you may learn a bit more about this by reading my artical here Raspberry PI:- USB power cables, crashing and other problems

    or here Raspberry PI:- USB, Ethernet, crashing and other problems | The Breadboard

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to Robert Peter Oakes

    So i may have looked over it but does having a higher amp 5v power source have any effect on the pi? Does more amps out of the power source help push voltage through the smaller wires?

     

    Also if you have two 5v connections coming in to a single usb cable does that mean its getting 10volts or still 5 volts but more amps?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to Robert Peter Oakes

    So i may have looked over it but does having a higher amp 5v power source have any effect on the pi? Does more amps out of the power source help push voltage through the smaller wires?

     

    Also if you have two 5v connections coming in to a single usb cable does that mean its getting 10volts or still 5 volts but more amps?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • uscdadnyc
    0 uscdadnyc over 10 years ago in reply to e14 Contributor

    AD wrote>>...

    Does more amps out of the power source help push voltage through the smaller wires?

    USCDADNYC>>No. The thickness (gauge size) of the wire determines the current (Amperage) carrying capacity of said wire. Do a Wiki on possible "current electricity"

    AD wrote>>...

    Also if you have two 5v connections coming in to a single usb cable does that mean its getting 10volts or still 5 volts but more amps?

    USCDADNYC>> No. You still have 5Volts. But the two 5Vdc power supply Bricks will fight each other. No two PSU (PSU = Power Supply Uinit= Pwr Bricks) are EXACTLY 5V. The lower voltage one will act as a Sink to the higher voltage one that acts as a Source. You could place a Diode between the two (if you try them together) BUT IT IS BEST THAT YOU KEEP THEM SEPARATE.

    USCDADNYC (NY NY USA)