Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Serial port appears to be controlled by another program.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 708 subscribers
  • Views 3765 views
  • Users 0 members are here
Related

Serial port appears to be controlled by another program.

tcoder
tcoder over 10 years ago

On a Raspberry Pi I have a program that was working great using the serial port /dev/ttyAMA0.  Now all of a sudden it doesn't work.  When I try and open the port, it only opens sometimes and when it doesn't, it hangs forever.  When I look at the port data with a logic analyzer, I get "ERROR" bytes coming from it.  I tried running "screen /dev/ttyAMA0 115200" and I get "ERROR login incorrect ERROR" messages.  It's as if some program has control over the port.  If I did something, I don't know what it was.  How can I find out what might be using the port besides me?

 

I decided to put an FTDI cable on the serial port and see what happens on a bootup.  Here is what I got:

 

[  380.473251] reboot: Restarting system

ERROR

Uncompressing Linux... done, booting the kernel.

ERROR

ø

ERROR

Welcome to the rescue system

ERROR

recovery login:

ERROR

Welcome to the rescue system

ERROR

recovery login:

ERROR

Welcome to the rescue system

ERROR

recovery login:

ERROR

Welcome to the rescue system

ERROR

recovery login:

 

How do I prevent the system from using the tty/AMA0 port?  I'm using it to connect to a Wifi module.

 

Terry

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    0 johnbeetem over 10 years ago

    I found this at RasPi Wiki at elinux.org:

    S/W: Preventing Linux from using the serial port

     

    By default Linux will grab the serial port and use it as a terminal. If you want to use it for other purposes you must prevent this. Here are the methods you can use: ...

    Maybe this is what's going on.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 10 years ago

    I found this at RasPi Wiki at elinux.org:

    S/W: Preventing Linux from using the serial port

     

    By default Linux will grab the serial port and use it as a terminal. If you want to use it for other purposes you must prevent this. Here are the methods you can use: ...

    Maybe this is what's going on.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • gdstew
    0 gdstew over 10 years ago in reply to johnbeetem

    You may be correct. There is a file in the boot partition/directory on the SD card called cmdline.txt. The file has one line in it:

     

    dwc_otg.lpm_enable=0 console=serial0,115200 console=tty1 root=/dev/mmcblk0p2 rootfstype=ext4 elevator=deadline fsck.repair=yes rootwait

     

    As you can see "console=serial0,115200" tells Linux to use the serial port as a console. If you remove that part of the command line (you probably

    want to save the original file in the boot directory first), Linux will no longer use the serial port. Since the boot partition uses a Microsoft FAT partition

    the file can be edited using either Windows or Linux.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tcoder
    0 tcoder over 10 years ago in reply to gdstew

    Thanks for all the help.  I decided to take another SD card and rebuild the system I had and save it as a starting point in case I have any other problems.  When I get finished, I'll go back to the original OS and figure out what caused the problem using the help you guys have given me.  I'm sure someone else might eventually have the same problem and would like to know what the resolution was.  Give me a day or so as I have other things to attend to.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tcoder
    0 tcoder over 10 years ago in reply to gdstew

    I pulled the SD card and looked at it.  There is no file called "cmdline.txt" on the disk.  Here is the contents of the SD card:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 10 years ago in reply to tcoder

    Not sure what OS you are using other than it is not Raspbian. I see the riscos-boot.bin file but the fact that you used raspi-config which is I believe a BASH

    script program to fix it has gotten me really confused.

     

    Good to see that you got it working !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tcoder
    0 tcoder over 10 years ago in reply to gdstew

    Actually, it's what came with the Pi I got from Element 14 along with the preconfigured SD card. I had two SD cards and they were both the same.