Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry pi doesn't work
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 23 replies
  • Answers 1 answer
  • Subscribers 707 subscribers
  • Views 4706 views
  • Users 0 members are here
  • not working
  • broken
  • raspberry_pi
Related

Raspberry pi doesn't work

ltimberlake
ltimberlake over 10 years ago

I received a raspberry pi 2 for my birthday from my parents, and I have tried multiple times to get it to work. I've tried installing multiple OS on multiple micro SD cards. I even bought a new power supply specifically for the raspberry pi even though the one i had before probably shoul've worked. The lights show up on the pi (red and green lights) but nothing shows up on the tv. I have tried multiple HDMI cords with multiple TVs. i have no receipt, what do you recommend i do?

  • Sign in to reply
  • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    short of the pi being broken, the most common issues are power and a bad SD card.

     

    Even if you have a good power supply, if it uses a separate USB lead then this also needs to be a good quality one. If the new PSU you got is the official one with integrated lead then this should be ok.

     

    You also need to get the latest image from raspberrypi.org and put this in a good class 10 SD card., with nothing plugged into the PI except the HDMI Screen, apply power

     

    you should get at least a rainbow on the HDMI screen and then it should start to boot., if the PSU is good and the SD card is a good class 10 version then it should work, if not then the chances are the board is faulty

     

    Where was it bought from, it may be replaceable under warranty if you have verified the above steps,

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • ltimberlake
    0 ltimberlake over 10 years ago in reply to Robert Peter Oakes

    There's not a separate usb lead, and what i bought was titled "raspberry pi power supply" and I confirmed that it works with pi 1,2, and 3. And Ive used multiple sd cards, so what should i do? can i get a new board if they sent me one that doesn't even work? Ill try one more sd card

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to ltimberlake

    If you are certain that the MicroSD card was properly inserted into the RPi2, then it might be that you need to have your parents contact whoever they bought it from.  There has to be an electronic trail somewhere.

     

    But, before you do that, I'd try to verify the MicroSD card and the HDMI cable on a known reliable computer or TV first:

    • Does the HDMI cable provide a functioning interface to your computer display or TV?
    • Can you mount the MicroSD drive as a removable drive on a computer at home using a caddy or some other MicroSD interface?

     

    If the HDMI cable and the MicroSD look good, then you probably have a "lemon" Pi.  Return it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • braedan
    0 braedan over 10 years ago

    I've had this problem too. What I did was not install the OS correctly, that may be your main problem. Is only the red light lighting up? That means there's power going to the pi. If so feel the cpu of the pi and if it can sting your finger after a couple of seconds then its bricked. :-{. If its not then celebrate! You probably just misinstalled the OS or didn't push the sd card in all the way.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Old OS SD image for Pi 1 do not boot at  next Pi versions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • uscdadnyc
    0 uscdadnyc over 10 years ago

    www.raspberrypi.org to obtain the version of Raspbian you want to download. www..bit.ly/win32sd to obtain latest(?) version of: win32diskimager-0.9.3-install. This is the program-app that writes the Raspian onto uSD/SD media. Again I ask comment(ers) to leave physical address (country residing it), b/c

    it is easier to trouble-shoot/solve/recommend possible solutions if we (all) Know what resources are available. I am a US-based Patent Atty, if you leave me w/ incomplete info, No problem, I will Bill you by the Hour, instead of a Flat Rate (for my services). Here at element14 we Comment(ers) do this for Gratis. Don't Make It Hard on Us to Help YOU. Full Disclosure: I am speaking as a Comment(er) NOT in any capacity representing element14

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royleith
    0 royleith over 10 years ago

    Hi Luke,

     

    I think the Raspi is working well. The problem is getting it to deliver an HDMI signal to the HDMI port.

     

    There is a config.txt file in the /boot partition which needs editing. Since the Raspi is not appearing on the screen, you will have to use another computer to edit the file.

     

    Hopefully, you have access to a computer that either has a slot for an SD or microSD card or you have a USB connected card reader. When viewed in a file manager, the config.txt file appears in its own partition with the label 'boot'. (Once booted in the Raspberry Pi, this folder appears as a /boot folder). The partition is formatted as FAT and can be viewed, and the files edited, in the same way as a flash drive.

     

    Use the text editor (Notepad, gedit, kate, etc.) that comes with the operating system. Don't use a word processor such as Microsoft Word or LibreOffice. Backup the default version of config.txt on the computer you are using so that you can always go back to the starting point.

     

    Each of the lines in the default config.txt come with an explanation of what it's for. Here are the lines you might want to edit.

     

    # uncomment if you get no picture on HDMI for a default "safe" mode

    #hdmi_safe=1

     

    # uncomment if hdmi display is not detected and composite is being output

    #hdmi_force_hotplug=1

     

    # uncomment to increase signal to HDMI, if you have interference, blanking, or

    # no display

    #config_hdmi_boost=4

     

    Try un-commenting (delete the #) the lines #hdmi_force_hotplug=1 and #config_hdmi_boost=4 so that they appear;

     

    # uncomment if hdmi display is not detected and composite is being output

    hdmi_force_hotplug=1

     

    # uncomment to increase signal to HDMI, if you have interference, blanking, or

    # no display

    config_hdmi_boost=4

     

    You should then get the HDMI screen to appear. If you are using a TV then you may then have to change the overscan settings to get the whole of the Raspi screen to be visible. If your TV has a 'computer monitor' mode, then use that (sometimes it appears in tv preferences as 'Overscan' settings). If you are using a monitor (or the TV equivalent), you will have a black border. Try,

     

    # uncomment this if your display has a black border of unused pixels visible

    # and your display can output without overscan

    disable_overscan=1

     

    Browse to

    RPiconfig - eLinux.org

    for a rather scarily detailed explanation of config.txt.

     

    I had the problem that a battery powered monitor kept making the Raspi boot into a very low resolution.

     

    The following configuration (in addition to the hotplug and boost lines above) makes the Raspi output a 16:9 PAL 1920x1080- 60Hz at the HDMI port:

     

    sdtv_mode=2

    sdtv_aspect=3

    hdmi_group=1

    hdmi_mode=16

    disable_overscan=1

     

    If that is not right for the TV  or monitor you are using, browse to the following,

     

    'config.txt' tag wiki - Raspberry Pi Stack Exchange

     

    Until you get the screen to display, you will have to power down the Raspi to remove the microSD card and re-edit the config.txt file. With luck, the Linux system will not be corrupted. Once you have the display working, always close Linux before powering down (Shutdown, in the Raspi applications launcher, bottom-Left).

     

    The application launcher also gives access to Raspberry Pi Configuration that may prove easier to make the changes than directly editing config.txt.  You may be able to get the configuration page by typing the following after launching Terminal using the Applications Launcher (see, above) ,

     

    sudo raspi-config

     

    It is possible to edit the file and then reboot from within the booted Raspberry Pi. You will need to run the text editor as 'super user'.

    sudo leafpad

     

    Edit the file and don't forget to save it.

     

    Choose Reboot in the Shutdown menu.

     

    If your Raspberry Pi ever asks for a password, try 'raspberry'. Your username is 'pi'.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • uscdadnyc
    0 uscdadnyc over 10 years ago

    This is about the RaspPi Zero. So if there-is a Moderator (of element14 community), feel free to move this comment to a more appropriate Thread. AAR this might be a Teachable Moment. i.e. my short 10min experience w/ RaspPi Zero. Teachable in both Substantive & Procedural Aspects. (Terms mostly associated w/ Law)AAR here goes: PROCEDURAL: (a) RaspPi Zero that has Camera Connector. (b) Micro USB OTG Hub (labeled For Smartphone and Tablet) . (c) USB KeyBd, (d) USB Mouse. (e) 16GB uSDcard w/ Raspbian Jessie-2016-05-27. SUBSTANTIVE: (Observations) HDMI Display shows booting OK. Get to RaspPi O/S GUI window, but the Keybd-[c] & the Mouse-[d] don't work. I know that [c] & [d] work b/c I took them off my working RaspPi 3B. This would point to (b) as the possible source of the problem(?) Will try another type of Powered USB2.0/3.0 Hub next. I also did a Wiki on OTG (On The Go) Hubs. No conclusion yet about whether I can use an OTG hub in this RaspPi Environment . BTW I ran power to the appropriate OTG connector- Still a Problem.

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • uscdadnyc
    0 uscdadnyc over 10 years ago in reply to uscdadnyc

    TS [Time Stamp] =13OCT16 1:52PM EDT. AAR an update. I have Not bought an OTG Adapter yet. But will also work along parallel line(s) to get this darn RaspPi Zero to work. Option (b) is via a Youtube video at url: https://www.youtube.com/watch?v=aL1pWI2K60w   This is a minimalist's dream you just need a PC, RaspPi Zero and a micro-B-plug-TO-full-size-USB-A-plug. (w/ full 4(5?) wires) AAR this is not w/o it's own problems. Although the video does not say to, I connected the HDMI to the RaspPi Zero and see that the RaspPi has trouble mounting /Root? AAR I will continue to post my Trials and trivialities. BUT I sure could use some help. All you need are the Three pieces of Equipment listed above.

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royleith
    0 royleith over 10 years ago

    Laptops are notorious for not supplying the full USB specified current (500mA?) to USB sockets, especially when in battery mode. Have you tried running your set-up from the rear USB ports of a desktop (some case mounted ports are under specification)?

     

    I appreciate that dragging the tower around slightly misses the point, but it will prove the viability of the Pi set-up.

     

    If the desktop works, try the laptop on mains power. If your laptop has USB 3, this might provide higher current.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>