Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Alternative for powerboost 500
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 705 subscribers
  • Views 1822 views
  • Users 0 members are here
  • power supply
  • raspberrypi_project
Related

Alternative for powerboost 500

e14 Contributor
e14 Contributor over 9 years ago

Hello,

 

I was searching for a cheaper alternative for the powerboost 500 and/or 1000. I came across this question on the forum but without an actual answer to it.

 

Basically i have a pi zero which i want to power with a lipo battery and add a charger board that can both charge the battery and be used as the power supply. I want to build an emulator machine that can but plugged into the wall while we play at home or that can be battery powered if i want to play it on the bus.

 

like i mentioned, the previous post I found about this question was referring to this board:

Li ion Lithium Battery Board Charger Module LED Board 5V 1A Mini USB Board | eBay

 

I'm not quite sure about the output pins, would they be b+, b- to charge the battery and out+, out- for the load?

 

Also, if anyone has any other inexpensive alternative I'm all ears.

 

Thanks in advance!

 

Pier

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 9 years ago

    Hi Pier,

     

    The module you've linked to will only do half the job; it will charge up a LiPo cell to 4.2V, but I think it won't convert to 5V. You'd also need a step-up DC-DC converter to provide you with 5V, or an all-in-one charger and DC-DC converver board maybe like this one. I don't know if 1A is sufficient for the pi-zero, nor if the board will actually supply 5V 1A or not, it was just the first one I saw on ebay.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 9 years ago

    Hi Pier,

     

    The module you've linked to will only do half the job; it will charge up a LiPo cell to 4.2V, but I think it won't convert to 5V. You'd also need a step-up DC-DC converter to provide you with 5V, or an all-in-one charger and DC-DC converver board maybe like this one. I don't know if 1A is sufficient for the pi-zero, nor if the board will actually supply 5V 1A or not, it was just the first one I saw on ebay.