Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum 1080 to 800x480
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 705 subscribers
  • Views 776 views
  • Users 0 members are here
  • raspberry_pi
Related

1080 to 800x480

e14 Contributor
e14 Contributor over 9 years ago

Hi everyone.

 

Just got my raspberri pi 3 model b with the 7 in touch display...

 

Im having difficulty setting the lcd to 800x480

Its still set to 1080 for some reason and im not getting full screen...

 

I tried

Sudo nano /boot/config.txt

And i un-hashed disable_overscan=1

 

Still no prevail

 

Besides that i added

lcd_rotate=2

Because the lcd case is upside down...

 

 

How can i set the pi lcd output to 800x480 resolution?

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago

    This should not be happening, with the latest firmware / OS image (Last few versions really), the LCD being the official PI one should configure perfectly right out of the box and should display full screen (With the exception of the upside down bit that is easy to remediate

     

    I have had to tweek things with non official displays that connect via the HDMI but then there's no surprise there.

    Have you tried the latest image from Raspberrypi.org and what was the result ?. If you got an SD card with the PI, don't trust it is the latest image, download the latest and re-flash the SD card.

    Peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago

    This should not be happening, with the latest firmware / OS image (Last few versions really), the LCD being the official PI one should configure perfectly right out of the box and should display full screen (With the exception of the upside down bit that is easy to remediate

     

    I have had to tweek things with non official displays that connect via the HDMI but then there's no surprise there.

    Have you tried the latest image from Raspberrypi.org and what was the result ?. If you got an SD card with the PI, don't trust it is the latest image, download the latest and re-flash the SD card.

    Peter