Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi Power Status LED Indicator
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 707 subscribers
  • Views 3146 views
  • Users 0 members are here
  • raspberry
  • status
  • help
  • pi
  • led
  • power
  • newbie
Related

Raspberry Pi Power Status LED Indicator

b8a
b8a over 9 years ago

Hey guys, I have recently gotten my new Pi 3.

I am loving it and am thinking of making myself a custom case for it.

However I have searched and searched and cannot for the life of me find out how I can wire up 2 LEDs in order to show the power status.

 

In other words, I want to find out how I can create a circuit that will have a red LED on when the Pi is off and a Blue LED on when the pi is on.

 

Thanks in advance.

 

PS: I am still quite new to the electrical  spectrum.

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 9 years ago

    I would try to get code that sets gpio pins for OS initialized and OS shutdown. See raspberry pi - Run code in python script on shutdown signal - Stack Overflow that will help. I leave for you how to turn on or off the actually lights. Nice idea BTW.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • b8a
    0 b8a over 9 years ago in reply to clem57

    I was thinking that as well.

     

    But I just do not know how to go about that.

     

    Would I be able to use the Pi's GPIO pins to select the LED by the high or low state of the GPIO?

    Is there a pin that is low when the pi is off and high when it is on?

     

    Thanks in advance

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to b8a

    That's a great idea for the push switch to safely turn the device off, something the raspberry pi would really benefit from! Once you export a gpio pin you can set the direction of the pin to be an output pin. Setting it's value to 1 will make it go high 3.3v and setting it to 0 will make it go low 0v. I haven't checked for certain but I would assume that the pins are always low when the raspberry pi is powered down so it should be simple enough to work a solution with indicator led's

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to b8a

    That's a great idea for the push switch to safely turn the device off, something the raspberry pi would really benefit from! Once you export a gpio pin you can set the direction of the pin to be an output pin. Setting it's value to 1 will make it go high 3.3v and setting it to 0 will make it go low 0v. I haven't checked for certain but I would assume that the pins are always low when the raspberry pi is powered down so it should be simple enough to work a solution with indicator led's

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer