Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum 1-wire temp sensor and serial input from tracer mppt solar controller
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 705 subscribers
  • Views 523 views
  • Users 0 members are here
  • raspberry_pi
Related

1-wire temp sensor and serial input from tracer mppt solar controller

linux51
linux51 over 9 years ago

i am using a Raspberry pi model B to log the data.  I had setup the 1-wire bus using this page https://www.modmypi.com/blog/ds18b20-one-wire-digital-temperature-sensor-and-the-raspberry-pi  and also using the on board serial on pin 8 and 10.  Both connections share the ground at pin 6.  The one 1-wire temperature sensor works and the serial connection from the solar charge controller work but the 1-wire sensor won't work with serial connected. With both connected under /sys/bus/w1/devices the sensor shows up with the wrong id and sometime multiples of the same id.  It his point I'm questioning where or not I have noise issue that is interfering with the 1-wire sensor.  Anybody have any ideas?  

  • Sign in to reply
  • Cancel
Parents
  • foxcam
    0 foxcam over 9 years ago

    Hello,

    I suggest to connect the DQ to the Pin 7 (GPIO 04). The 1 wire does not communicate via the serial port.

    After the configuration is done Raspberry will store the results as follow (28-.. as an example): /sys/bus/w1/devices/28-00000482b243

    Good luck! Felix

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • foxcam
    0 foxcam over 9 years ago

    Hello,

    I suggest to connect the DQ to the Pin 7 (GPIO 04). The 1 wire does not communicate via the serial port.

    After the configuration is done Raspberry will store the results as follow (28-.. as an example): /sys/bus/w1/devices/28-00000482b243

    Good luck! Felix

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer