Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum What is the case included in the IoT Learner kit?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 703 subscribers
  • Views 637 views
  • Users 0 members are here
  • raspberrypi.
  • raspberry_pi
Related

What is the case included in the IoT Learner kit?

martiserrano
martiserrano over 9 years ago

What is the case included in the IoT Learner kit? I already have a Raspberry PI and just want the sense Hat and the case

  • Sign in to reply
  • Cancel
  • clem57
    0 clem57 over 9 years ago

    Raspberry Pi 3 features:

     

    • Quad Core 1.2GHz Broadcom BCM2837 64bit CPU
    • 1GB RAM
    • BCM43438 WiFi and Bluetooth Low Energy (BLE) on board
    • 40-pin Extended GPIO
    • 4x USB 2 ports
    • 4 Pole stereo output and composite video port
    • Full size HDMI
    • CSI camera port for connecting a Raspberry Pi camera
    • DSI display port for connecting a Raspberry Pi touchscreen display
    • Micro SD port for loading your operating system and storing data
    • Upgraded switched Micro USB power source up to 2.5A

     

    Sense HAT features:

     

    • Official Sense HAT from the Raspberry Pi Foundation
    • 8x8 LED matrix display
    • Accelerometer, gyroscope and magnetometer
    • Air pressure sensor
    • Temperature and humidity sensor
    • Small joystick

     

    Power Supply Features:

     

     

    • 1.5m Micro USB
    • 4 changeable heads for use in the UK, Europe, Australia & US regions
    • Current rating : 2.5A

     

    Raspberry Pi Case features:

     

    • Designed to house the Raspberry Pi B , Raspberry Pi 2, Raspberry Pi 3 and HAT PCBs
    • HAT can be removed without removing the Raspberry Pi from the enclosure
    • All cut-outs are pre-cut into the case
    • Camera ribbon slot in enclosure lid
    • Display ribbon slot in enclosure lid
    • Label recess on enclosure base
    • Gloss finish

    Which shows out of stock. Why not get Raspberry Pi Sense HAT (plenty in stock) and a case for less than $50.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • martiserrano
    0 martiserrano over 9 years ago in reply to clem57

    Hi Clem,

    that's my point, geting the sense + case but want a case that fits both, Raspi and Sense, hence my question.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 9 years ago in reply to martiserrano

    I can not say here the exact one, but I would look at Amazon for the case searching for case raspberry pi sense