Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum connect pi V3 to gertboard V1
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 2 answers
  • Subscribers 707 subscribers
  • Views 895 views
  • Users 0 members are here
  • raspberry_pi
Related

connect pi V3 to gertboard V1

ptou666
ptou666 over 9 years ago

I am very much a newbie to the Pi and some time ago I bought an original Gertboard to play with.  I assembled the Gertboard but then domestic problems caused me to lay the project aside.

I now have purchased a new Pi (V3) and when I went to connect the two I found that the connectors had changed from the original ribbon cable to a direct connection.

I would still like to use my old Gertboard with my new Pi, but I am afraid to guess at the connection required - is it possible to do this please?

  • Sign in to reply
  • Cancel
Parents
  • gdstew
    0 gdstew over 9 years ago

    The first 26 pins on the Pi 3 interface connector are the same as the 26 pins on the Gertboard interface connector so as long as you make sure

    to connect pin 1 on the cable from the Gertboard to pin 1 of the connector of the Pi it will be OK. The Gertboard test software written for the

    original Pis will not work on the Pi 3 ( or Pi 2) because a couple of the I/O pins were changed and the addresses of the I/O pins and other interfaces

    (serial, I2C, SPI) was changed when they started shipping with 1 GB of RAM. The different addresses used and the pin changes should be fairly

    easily to fix in the test software.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • gdstew
    0 gdstew over 9 years ago

    The first 26 pins on the Pi 3 interface connector are the same as the 26 pins on the Gertboard interface connector so as long as you make sure

    to connect pin 1 on the cable from the Gertboard to pin 1 of the connector of the Pi it will be OK. The Gertboard test software written for the

    original Pis will not work on the Pi 3 ( or Pi 2) because a couple of the I/O pins were changed and the addresses of the I/O pins and other interfaces

    (serial, I2C, SPI) was changed when they started shipping with 1 GB of RAM. The different addresses used and the pin changes should be fairly

    easily to fix in the test software.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • ptou666
    0 ptou666 over 9 years ago in reply to gdstew

    Hi Gary,

    Many thanks for this; as I've said to Clem, I can now connect up my old board with some confidence that it won't go up in smoke.

    Thanks again,

    Pat