Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Power Supply Question
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 21 replies
  • Answers 8 answers
  • Subscribers 708 subscribers
  • Views 4050 views
  • Users 0 members are here
  • power supply
  • multiple_output
  • raspberry_pi
  • raspberry pi 3 model b
Related

Power Supply Question

finian826
finian826 over 9 years ago

Good day,

 

Can anyone recommend a good power supply to power 4 or 5 model 3 Pi's? Or can anyone point to a hack with a computer power supply wiring to multiple usb jacks?

 

Any info would be great. I don't want to run a single power bar for just power bricks for my Pi's.

 

Thanks

Terry

  • Sign in to reply
  • Cancel
Parents
  • rew
    0 rew over 9 years ago

    A "cheap" hack, requiring some "DIY" is to use a standard (small?) ATX powersupply. The "5Vstandby" is enough to power one pi (i.e. silent!), you need to turn the supply on to power more than one. I would personally not hesitate to make a harness that connects to the GPIO pins, so that I can bypass USB cables to be sure that I don't run into bad ones (i.e. having a large resistance).

     

    On my desk, for testing, I have an ATX powersupply that is "ON", but I have patched the fan to run off 5V instead of the normal 12V. I'm guessing that this reduces the total allowed  power output from the 500W it is rated at to below 100W or so, but it is currently powering two raspberry PIs and a couple of other projects...... (say 5W for the pi's (on average, 10W peak each) and another 5W for the rest....)

     

    So.... Another option is to do what I did: get that ATX powersupply, and route the 5V through thick cables to a big enough (cheap! (*)) USB hub, and just use the hub to distribute the power.

     

    (*) The hub needs to be cheap enough that it simply passes on the power instead of being intelligent about it and only delivering the required 0.1A until the client negotiates more.... 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • rew
    0 rew over 9 years ago

    A "cheap" hack, requiring some "DIY" is to use a standard (small?) ATX powersupply. The "5Vstandby" is enough to power one pi (i.e. silent!), you need to turn the supply on to power more than one. I would personally not hesitate to make a harness that connects to the GPIO pins, so that I can bypass USB cables to be sure that I don't run into bad ones (i.e. having a large resistance).

     

    On my desk, for testing, I have an ATX powersupply that is "ON", but I have patched the fan to run off 5V instead of the normal 12V. I'm guessing that this reduces the total allowed  power output from the 500W it is rated at to below 100W or so, but it is currently powering two raspberry PIs and a couple of other projects...... (say 5W for the pi's (on average, 10W peak each) and another 5W for the rest....)

     

    So.... Another option is to do what I did: get that ATX powersupply, and route the 5V through thick cables to a big enough (cheap! (*)) USB hub, and just use the hub to distribute the power.

     

    (*) The hub needs to be cheap enough that it simply passes on the power instead of being intelligent about it and only delivering the required 0.1A until the client negotiates more.... 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer