Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Power Supply Question
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 21 replies
  • Answers 8 answers
  • Subscribers 708 subscribers
  • Views 4054 views
  • Users 0 members are here
  • power supply
  • multiple_output
  • raspberry_pi
  • raspberry pi 3 model b
Related

Power Supply Question

finian826
finian826 over 9 years ago

Good day,

 

Can anyone recommend a good power supply to power 4 or 5 model 3 Pi's? Or can anyone point to a hack with a computer power supply wiring to multiple usb jacks?

 

Any info would be great. I don't want to run a single power bar for just power bricks for my Pi's.

 

Thanks

Terry

  • Sign in to reply
  • Cancel
Parents
  • rsc
    0 rsc over 9 years ago

    I've found that my Pi-3 needs about 5.2VDC to operate properly with a WD pi-drive and regular sized keyboard and mouse.

    The supply I built for testing this has an adjustable 5V output. It's a Mean Well RD-50B dual output 5V@4A and 24V@1.4A

    http://www.onlinecomponents.com/mean-well-rd50b.html?p=11952931

    I added a fuse and current meter to monitor what's happening.

    Here's a pic

    image

    Scott

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to rsc

    Until now, the most reliable solution to give a good power to a consistent project (like the modules I am doing for the PiIoT MuZIEum project is using ATx power supplies.

    The only doubt I have is if it is reliable just to shortcut the power pin to make the unit working properly or some kind of circuit should be done, like an emulation of the logic power button on the PC

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Workshopshed
    0 Workshopshed over 9 years ago in reply to balearicdynamics

    I've used a couple of ATX power supplies like that for running extractor fans in the workshop. So far have proved reliable but are only on for a few hours at a time. I can't see why you would need a special circuit, it is just a signal line that you have to pull low.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to Workshopshed

    It is true... I have read somewhere that the. Atx can be damaged just short circuit the power pin to gnd witjout a resistor... Better to solder just a cable image

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to Workshopshed

    It is true... I have read somewhere that the. Atx can be damaged just short circuit the power pin to gnd witjout a resistor... Better to solder just a cable image

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Workshopshed
    0 Workshopshed over 9 years ago in reply to balearicdynamics

    The kit versions for adapting ATX to bananna plugs often have a space for a high current load resistor to place across the output. I believe it will help stabalise the output voltage as most of these supplies are switch mode. Best not short the outputs though!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to Workshopshed

    So you confirm that a resistor should be placed between the ATX power pin (the green one) and one of the GN pins with a resistor between. What value do you suggest?

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 9 years ago in reply to Workshopshed

    Not sure if it is still the case or not but a number of SMPS designs used to require a minimum load on the output in order to operate correctly. I'd hazard a guess that the space for the load resistor may be for this purpose, especially if being used as a bench supply where the load may not always meet the minimum load requirement of the SMPS.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rew
    0 rew over 9 years ago in reply to beacon_dave

    Yes, for both "switching powersupplies" and "atx power supplies" stories are going around that they require a lot to operate correctly. One of the devices where you wouldn't expect it are some MEANWELL power supplies. There it seems to me that they no longer guarantee that the output will remain within 5% of the nominal value if the output is unloaded. Not really a problem if you can tolerate say +10%. Just being able to cope with 13.2V is much cheaper in the long run than adding a load resistor.

     

    Similarly, some old ATX power supplies would give weird results, like the 5V rising to 6V or more when only the 12V was loaded. I haven't seen such "weird" behaviour from any supply made the last two decades. (I used to say I had never seen it, but that is no longer true. A few years ago, I grabbed an older  powersupply from the pile of "old spare powersupplies" and it indeed behaved weird and required a load to be stable. That powersupply was built in 1992. )

     

    In practice, it isn't a problem or only happens with very old/odd equipment.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 9 years ago in reply to balearicdynamics

    Some power supplies need a load resistor on the power output to be stable, but I have re-purposed 3 PC power supplies using a custom PCB with banana sockets, fuses and switches. The card I designed has room for power resistor loads, but in every case the output voltages were accurate and stable without any load. The power switch just controls the power control signal. Maybe I will post a blog about it....

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to dougw

    It will be very helpful ... Thanks in advance

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Workshopshed
    0 Workshopshed over 9 years ago in reply to balearicdynamics

    You can twist green and GND together or have a switch if you want.

    The load is from 5v to GND.

     

    http://www.electronics-tutorials.ws/blog/convert-atx-psu-to-bench-supply.html

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to Workshopshed

    Very clear Andy! Thank you for the precious suggestions.

     

    Enrico