h
Start small with 2 or 3 and add later when needs and money dictate.
Thanks I will do that first. Thanks!!!
Just an after thought, you may want to consider the Pi Zero. It only has one core, but they take less space. At $5 dollars apiece at Micro center, not a bad deal. Once catch, they only sell one at a time. You will also need to solve the lack of Ethernet and only micro USB connection. But that makes the project more fun solving the engineering problems.
You've got a funny idea there, clem! For "computing" there is not much "external" stuff you need except for a networking connection. So just plugging a cheap ethernet adapter into each pi zero should do the trick. Get yourself a TTL-serial adapter for configuration and debugging until the ethernet works....
You've got a funny idea there, clem! For "computing" there is not much "external" stuff you need except for a networking connection. So just plugging a cheap ethernet adapter into each pi zero should do the trick. Get yourself a TTL-serial adapter for configuration and debugging until the ethernet works....
Yes I agree. That was precisely what I was going to do. Thanks!!!