Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum What operating system should I use to connect my iPad with iTunes?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 3 answers
  • Subscribers 707 subscribers
  • Views 1608 views
  • Users 0 members are here
  • ipad
Related

What operating system should I use to connect my iPad with iTunes?

unsagicois
unsagicois over 9 years ago

What operating system should I use in the Raspberry to install iTunes and connect my iPad to sync? Can the Windows 10 loT accept the latest version of iTunes? Or, is there any other program like iTunes or file maneger program that will read the file system of the iPad?

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 9 years ago

    Since iTunes is written for Intel and the source is not available, it is not possible to run on RPi since it it ARM based. But there are alternatives looking at 10 Alternatives to iTunes for managing your iPod - Simple Help . These run on on Windows(full not IOT), open source, or Linux. Give one or two a whirl.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • unsagicois
    0 unsagicois over 9 years ago in reply to clem57

    I just recently got my raspberry pi started. I had a few of those alternatives to iTunes installed, but I'm certain now that is not what I'm looking for.

    I NEED TO READ AND EDIT THE SYSTEM FILES OF MY IPAD AND OF ANDROID CELLPHONES LIKE SAMSUNG.

    i need a file manager like "iFile".

    what programs can I download?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • the-dubster
    0 the-dubster over 9 years ago in reply to unsagicois

    Unfortunately I have been unable to find ANY that do what you want. Anapod Explorer used to do it, you could essentially use your iPod like an external drive (or at least access the file structure) but Apple get a little twitchy about things like that.

    There may be options I have not tried, a good 'googling' may turn something up.

     

     

                                                      (As for iTunes being written for Intel - I was going to comment that I was using it on my Mac - then I remembered that my Mac runs an Intel i5 Processor! oops)!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to unsagicois

    Im not sure exactly what you want to do with it but the following webpage suggests a way to use filezilla to read and transfer files over a wifi connection https://dottech.org/18890/four-ways-to-access-your-idevices-iphoneipadipod-touch-file-system-from-your-computer/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • the-dubster
    0 the-dubster over 9 years ago in reply to e14 Contributor

    That does require a jailbroken device - something I've never been willing to do.

     

    It used to be possible without jailbreaking - Apple being rather protective has seemingly put a kybosh on that.

     

    The post that you linked is 7 years old - but it may still work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • unsagicois
    0 unsagicois over 9 years ago in reply to e14 Contributor

    I need to remove the password in the Restrictions of the General menu. I did not forget the password. This is happened on my old iPad asWeill as the new one. It just fails to accept the password I've often using.

    The is a hacker instruction to edit the plist, but they suggested using "backupbot", however it I used ion with my iFile on the jailbreak old iPad and it worked fine. But my new iPad is not jailbroken.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • unsagicois
    0 unsagicois over 9 years ago in reply to e14 Contributor

    I need to remove the password in the Restrictions of the General menu. I did not forget the password. This is happened on my old iPad asWeill as the new one. It just fails to accept the password I've often using.

    The is a hacker instruction to edit the plist, but they suggested using "backupbot", however it I used ion with my iFile on the jailbreak old iPad and it worked fine. But my new iPad is not jailbroken.