Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum There is a broken chip on my Rpi3 motherboard labeled: 4R7. I just bought it and it broke while trying to install it inside the case. Will the board still work with that chip broken? Can I cover it with epoxy?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 12 answers
  • Subscribers 708 subscribers
  • Views 13507 views
  • Users 0 members are here
  • broken chip
Related

There is a broken chip on my Rpi3 motherboard labeled: 4R7. I just bought it and it broke while trying to install it inside the case. Will the board still work with that chip broken? Can I cover it with epoxy?

unsagicois
unsagicois over 9 years ago

There is a broken chip on my Rpi3 labeled: "4R7". I just bought it and it broke while while trying to install inside the case.

Will that chip: "4R7 being cracked will prevent the Rpi3 from working properly? Can I simply coat the chip with epoxy?

This is my first experience with Raspberry. I never heard of it before until I saw an advertisement for Cayenne in Facebook last month.

image

  • Sign in to reply
  • Cancel
Parents
  • COMPACT
    0 COMPACT over 9 years ago

    Epoxy is not conductive so just get someone with the right equipment to replace it to ensure it'll work properly.

    The price of the 4k7 is very cheap - can be low as fractions of cents.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rew
    0 rew over 9 years ago in reply to COMPACT

    Dear Compact,

    You are thinking of a resistor. The resistors on the raspberry pi are mostly so small that they do not have a marking. There are however two inductors prominently marked "4R7".  Resistors cost factions of a cent, the cheapest inductors that I can find are about 10 cents.


    Most before me haven't mentioned it, but the cracked component is not a chip, not a resistor but an inductor.

     

    The two inductors are involved in the power circuit. They make, I believe, 3.3V and 1.8V from the 5V input. Because they step the voltage down, I can predict how they are wired. If the inductor is broken, one of those power rails will simply remain at 0V. This COULD damage one of the chips on your raspberry, but it is unlikely.

     

    The inductor consists of a wire wrapped around a core. If that core is cracked, the inductor will not work as well as it should. On the other hand, it is usually not all that critical in the power circuit, so if things change a bit due to the crack there is a possibility that things still work. The continuity of the wire is essential though. So... if you power up your pi, and it works, then that continuity is ensured. In that case encasing it with epoxy might work. On the other hand, if it fails after you epoxy it, it will be impossible to fix.

     

    Replacing an SMD component is easy enough if you have the right tools. But having those tools and knowing how to use them is not trivial.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • COMPACT
    0 COMPACT over 9 years ago in reply to rew

    Michel,

     

    Sorry, my mistake. It is actually shorthand for an Bourns SRN4018-4K7M 4.7uH (microhenry) inductor (or equivalent) and has a huge price tag of 13 US cents.

    So I'd replace it if it is cracked through the centre.

    No real worries if it's just a little bit of a corner.

    You can test the inductor to see if its coil is intact. When measured with a multimeter it'd read 0 ohms if ok (with the Pi turned off!).

     

    When the ferrite is in operation it is under mechanical stress from the constant charging and discharging.

    Epoxy is used to reduce buzzing from inductors but the epoxy is of a type not to affect its heat dissipation.

     

    If you play your cards right with an inductor manufacturer you may be able get one as a sample - Zero Cents!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rew
    0 rew over 9 years ago in reply to COMPACT

    IMHO the cost of the component is irrelevant.

     

    Before Michel is able to replace the inductor the costs are many, many times more than just the 13 cents for the inductor.

     

    * Buy, or arrange to borrow the right desoldering equipment.

    * find time to desolder the component.

    * manage to solder on the new one without damage to the surrounding components.

     

    Factor in the chances of ruining the pi for good (IMHO about 50/50), the costs are WAY more than the 13 cents for the inductor. So his idea of epoxying the component in place sounds like the better bet. Just first test if the pi still works. Then you can be confident that it is electrically OK. Then apply the epoxy. (Because Michel comes with the suggestion of epoxy, I'm assuming that's easy for him because he has all the stuff to do that.)

     

    If the pi no longer works, it's a dead board. You can do anything with it, even: try to repair it. However, the replacing the inductor on a pi is not the easiest of "first projects" to try and learn such a task....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • COMPACT
    0 COMPACT over 9 years ago in reply to rew

    Very Compact wrote previously:

     

     

    Epoxy is not conductive so just get someone with the right equipment to replace it to ensure it'll work properly.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • unsagicois
    0 unsagicois over 9 years ago in reply to COMPACT

    I had to get some sunshine to get a good pic. It is the L2 - 4R7. The ohm meter reads 10 ohms, unless I'm reading it wrong, but it is not zero anyway. It does not look like the wires are broken or the contacts loose. I will not apply any power to this until I am sure there will be no further damage to the circuits. I have soldering equipment but I am not very proficient at soldering, but I have a friend how is more experienced at it than I am. Otherwise, I doubt I will find a replacement since I am stranded here in the boondocks of Asia, namely a province in the Philippines (pun intended). I thought it was a heat sink of some kind, so I have to ask to make sure if epoxy was safe to use. I really, really need this to work. It is my only chance. Thanks.

     

     

    image

     

    image

     

    Sent from my iPad

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • unsagicois
    0 unsagicois over 9 years ago in reply to COMPACT

    I had to get some sunshine to get a good pic. It is the L2 - 4R7. The ohm meter reads 10 ohms, unless I'm reading it wrong, but it is not zero anyway. It does not look like the wires are broken or the contacts loose. I will not apply any power to this until I am sure there will be no further damage to the circuits. I have soldering equipment but I am not very proficient at soldering, but I have a friend how is more experienced at it than I am. Otherwise, I doubt I will find a replacement since I am stranded here in the boondocks of Asia, namely a province in the Philippines (pun intended). I thought it was a heat sink of some kind, so I have to ask to make sure if epoxy was safe to use. I really, really need this to work. It is my only chance. Thanks.

     

     

    image

     

    image

     

    Sent from my iPad