Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Velleman K2633 Relay Card Troubleshooting
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 4 answers
  • Subscribers 708 subscribers
  • Views 1945 views
  • Users 0 members are here
  • raspberry_pi
Related

Velleman K2633 Relay Card Troubleshooting

mattwilliams
mattwilliams over 9 years ago

Good day.

 

I get unexpected results when connecting a K2633 relay card to my Raspberry Pi 3 and hope someone can help.

 

When my Python 3 code sends 3.3V from any GPIO pin to any IN pin on K2633, the K2633 LED on that channel lights, but that relay does not energize. This occurs when the K2633 is supplied with either 5VDC from the RPi or 9VDC from a separate and isolated supply.

 

The four K2633 SPDT relays are 6V units. K2633 product literature calls for a 9V power supply - which I have. I realize that 5V from RPi is not enough voltage to energize the relays.

 

K2633 is built correctly and any relay can be forced to function properly by supplying 9VDC to the K2633 and shorting any IN pin to GND. In such a case, that particular relay will energize. Do I need to program an RPi GPIO pin to go to GND when I want to energize the relay? If so, I am not aware of how this is possible - since I understand output pins to only be capable of either zero or 3.3V when defined as outputs - with zero volts not meaning 'connected to GND'. Do I correctly understand this item?

 

This is a breadboard setup for proof of concept to control any relay and with nothing presently connected to C, NO or NC terminals, so final switching application is unrelated to problem. Final application will be to switch a US 110 VAC / 90 Watt ceiling fan on and off. The fan's power ratings are within the relays' capabilities of 15 A / 125 VAC. Is a different relay card a better choice?

 

RPi and code function properly - since I can turn on and off an LED with the circuit / program in addition to seeing 3.3V at any K2633 IN pin with a multimeter.

 

Thank you for any direction you might be able to offer.

 

Matt

  • Sign in to reply
  • Cancel
Parents
  • mcb1
    0 mcb1 over 9 years ago

    The linked schematic is a bit blurry but if I read it right it uses PNP transistors that feed the 9v to the coil.

    This means the base of the transistor will be about 8.3v and far too high for the Raspberry Pi.

     

    You'll need to add a transisor or an optocoupler between the RPi GPIO and the relay control pin.

     

     

    Do I need to program an RPi GPIO pin to go to GND when I want to energize the relay?

    Yes you will BUT you cannot connect the 8.3v input to the RPi GPIO.

    This is referred to as ACTIVE LOW meaning the circuit is active/on when it is low.

     

    The ground of the supply for the relay and the RPi ground should be connected, and then when the GPIO is LOW it would turn ON

    BUT again with the 8.3v you shouldn't.

     

    If you use an optocoupler you wouldn't need to connect the two.

     

     

    Hope this helps.

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 9 years ago

    The linked schematic is a bit blurry but if I read it right it uses PNP transistors that feed the 9v to the coil.

    This means the base of the transistor will be about 8.3v and far too high for the Raspberry Pi.

     

    You'll need to add a transisor or an optocoupler between the RPi GPIO and the relay control pin.

     

     

    Do I need to program an RPi GPIO pin to go to GND when I want to energize the relay?

    Yes you will BUT you cannot connect the 8.3v input to the RPi GPIO.

    This is referred to as ACTIVE LOW meaning the circuit is active/on when it is low.

     

    The ground of the supply for the relay and the RPi ground should be connected, and then when the GPIO is LOW it would turn ON

    BUT again with the 8.3v you shouldn't.

     

    If you use an optocoupler you wouldn't need to connect the two.

     

     

    Hope this helps.

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer