Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum How to add Romex Cable to this Junction Box
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 4 answers
  • Subscribers 708 subscribers
  • Views 5024 views
  • Users 0 members are here
  • 120v
  • romex
  • ac
  • ac outlet
  • raspberry_pi
  • power
  • home
Related

How to add Romex Cable to this Junction Box

gub11
gub11 over 9 years ago

I live in the US. I am trying to install an ac outlet in my attic. Attached is a metal junction box that looks like it has Romex cable coming out of it. However, the cables go straight to either lights, or other rooms, so how can I add a Romex cable to that junction box? Maybe there is a standard procedure or a diagram that I'm unaware of. And before you all say "hire an electrician, ac voltage is dangerous" I will cut the power to my house completely beforehand, and, for a bit of extra safety, wear rubber gloves and keep 1 hand behind my back. https://www.youtube.com/watch?v=1O85YSd8Vts

  • Sign in to reply
  • Cancel
Parents
  • holmziep
    0 holmziep over 9 years ago

    Dennis and John have some good advice:  I should of let things be, but I wrote this so I am gona post it anywhere, as long winded as it is!

     

    Holy sparks, Gabriel: You should have a meter to measure 120 / 240 volts AC.  You need to take off the cover, loosen one screw and remove the other.  You will see the wires connected together with wire nuts.  Hopefully there are 3 white (neutral) and 3 black (hot) wires, and 3 ground wires, each connected together with their own wire nuts.  (If not, OR if you see a red wire, STOP and study, there may be a switch or something.  You are looking for a simple 120 Volt AC circuit, right?)  If you are lucky, the older metal BX cable may be an original feed (already with lots if stuff on it?) from an existing circuit, originating from the service panel.  The two romex cables were run at some later time feeding lighting or receptacles?  Follow the wires, especially the "Newer" romex, down where they protrude into the wall below and do your best guess on where they go. Lights? Switches? Outlets?  If one wire looks like it goes to a switch, it disconnects the HOT (black) wire going to a light, so be aware.  Do some good reasoning. Read about residential wiring  Once your have a best guess, you should then go down and identify the breaker that controls THAT circuit somehow.  Sometimes the breakers are MARKED within the service panel, making it obvious. 

     

    The Breaker MUST normally correspond to the gauge of the wire you have to use:  14 gauge for 15 amp circuits, and 12 gauge wire for 20 amp circuits.  The Romex wire you use must be the minimal gauge.  You need 14-2 with ground, or 12-2 with ground, having a black and a white conductor, and a bare copper ground.   NOT 12-3 or 14-3!   Also check the existing romex wire markings, they should say 14- 2 or 12-2 with ground, and correspond with the breaker feeding the circuit.  Be aware that the person adding the new circuits may of not been an electrician, and wanted to use the "cheaper" 14-2 with ground on a 20 amp circuit which is illegal and dangerous.  That'ts why we are ELECTRICIANS!

     

    Again, Gabe:  You need to be sure your dealing with 120 volts AC, uses your meter to test between a white wire and the black wire.  You would use ROMEX or equivalent wire, of the proper gauge.   They call the stupid clamps  that hold the wires to the box "connectors" for some reason, there are plastic ones and metal ones made for 1 or 2 romex cables.

     

    DON't turn off the MAIN BREAKER, gosh, Gabe!

     

    WITH THE CIRCUIT BREAKER OFF:  You add another wire to that 4" square junction box.  You may even be able to use the existing wire nuts, or use larger wire nuts inside to accommodate the larger number of wires.  Locate and tap out a small knockout the same size used for the romex, remove the sheathing from the romex about 6", and take about 5/8 inch of insulation off the black and white wires.  Connect the black to black (hot) and the white to white (Neutral) using wire nuts .   Connect all the bare copper ground wires together with a wire nut.  Hopefully you see the metal box also has a bare copper ground wire included with the bunch.

     

    Receptacles have the same arrangement.  Decide how you want to attach a single or double receptacle box to the floor, wall, ceiling, rafter, and select a box that mounts that way.  Some plastic boxes have built in clamps, and some metal boxes do to, but if not, you will have to have clamps (oh, yah, "connectors")  On the recepticles, the silver colored screws are for the white wire, the brass colored screws are for the black (hot) wire, and the green screw is for the copper wire.  Get a face plate for your box.

     

    Go to Home Depot if you have that around, or your local home supply store, and dig around.  Read. Watch YouTubes.  Do it Right.

     

    Gabe:  Electricians make LOTS of MONEY and get very dirty doing it.  It beats living in the basement 'till you're 32.

     

    Pete, N2EXG

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • holmziep
    0 holmziep over 9 years ago

    Dennis and John have some good advice:  I should of let things be, but I wrote this so I am gona post it anywhere, as long winded as it is!

     

    Holy sparks, Gabriel: You should have a meter to measure 120 / 240 volts AC.  You need to take off the cover, loosen one screw and remove the other.  You will see the wires connected together with wire nuts.  Hopefully there are 3 white (neutral) and 3 black (hot) wires, and 3 ground wires, each connected together with their own wire nuts.  (If not, OR if you see a red wire, STOP and study, there may be a switch or something.  You are looking for a simple 120 Volt AC circuit, right?)  If you are lucky, the older metal BX cable may be an original feed (already with lots if stuff on it?) from an existing circuit, originating from the service panel.  The two romex cables were run at some later time feeding lighting or receptacles?  Follow the wires, especially the "Newer" romex, down where they protrude into the wall below and do your best guess on where they go. Lights? Switches? Outlets?  If one wire looks like it goes to a switch, it disconnects the HOT (black) wire going to a light, so be aware.  Do some good reasoning. Read about residential wiring  Once your have a best guess, you should then go down and identify the breaker that controls THAT circuit somehow.  Sometimes the breakers are MARKED within the service panel, making it obvious. 

     

    The Breaker MUST normally correspond to the gauge of the wire you have to use:  14 gauge for 15 amp circuits, and 12 gauge wire for 20 amp circuits.  The Romex wire you use must be the minimal gauge.  You need 14-2 with ground, or 12-2 with ground, having a black and a white conductor, and a bare copper ground.   NOT 12-3 or 14-3!   Also check the existing romex wire markings, they should say 14- 2 or 12-2 with ground, and correspond with the breaker feeding the circuit.  Be aware that the person adding the new circuits may of not been an electrician, and wanted to use the "cheaper" 14-2 with ground on a 20 amp circuit which is illegal and dangerous.  That'ts why we are ELECTRICIANS!

     

    Again, Gabe:  You need to be sure your dealing with 120 volts AC, uses your meter to test between a white wire and the black wire.  You would use ROMEX or equivalent wire, of the proper gauge.   They call the stupid clamps  that hold the wires to the box "connectors" for some reason, there are plastic ones and metal ones made for 1 or 2 romex cables.

     

    DON't turn off the MAIN BREAKER, gosh, Gabe!

     

    WITH THE CIRCUIT BREAKER OFF:  You add another wire to that 4" square junction box.  You may even be able to use the existing wire nuts, or use larger wire nuts inside to accommodate the larger number of wires.  Locate and tap out a small knockout the same size used for the romex, remove the sheathing from the romex about 6", and take about 5/8 inch of insulation off the black and white wires.  Connect the black to black (hot) and the white to white (Neutral) using wire nuts .   Connect all the bare copper ground wires together with a wire nut.  Hopefully you see the metal box also has a bare copper ground wire included with the bunch.

     

    Receptacles have the same arrangement.  Decide how you want to attach a single or double receptacle box to the floor, wall, ceiling, rafter, and select a box that mounts that way.  Some plastic boxes have built in clamps, and some metal boxes do to, but if not, you will have to have clamps (oh, yah, "connectors")  On the recepticles, the silver colored screws are for the white wire, the brass colored screws are for the black (hot) wire, and the green screw is for the copper wire.  Get a face plate for your box.

     

    Go to Home Depot if you have that around, or your local home supply store, and dig around.  Read. Watch YouTubes.  Do it Right.

     

    Gabe:  Electricians make LOTS of MONEY and get very dirty doing it.  It beats living in the basement 'till you're 32.

     

    Pete, N2EXG

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • gub11
    0 gub11 over 9 years ago in reply to holmziep

    Thanks for the very in depth description.  I just went up and opened the 4" square junction box, but the wires aren't connected to the same color.  I see black to white and red to black and there is a blue wire.  There is are two metal tubes with wires feeding into it and 1 romex feeding out of it.  What should i be looking for?