Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Is the element14 Desktop enclosure compatible with GPIO add-on cards?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 707 subscribers
  • Views 1068 views
  • Users 0 members are here
  • ups
  • gpio
  • ups-pico
  • add-on-board
  • raspberry_pi
  • pi desktop
Related

Is the element14 Desktop enclosure compatible with GPIO add-on cards?

jdb2
jdb2 over 9 years ago

Hello. I've been thinking of getting an Element14 Raspberry Pi Desktop enclosure for my RPi 3, but, I need to know if the enclosure is compatible with the UPS-Pico GPIO add-on board ( UPS PIco HV3.0A Stack Plus with 450mAh Battery  ). I've called Newark/element14 tech support, but the support rep didn't have a definitive answer as even he couldn't find any dimensions for the Desktop enclosure.

 

Any help regarding this topic or how to possibly get around the space constraints, if possible, would be greatly appreciated.

 

EDIT : Stupid oversight on my part -- I missed the dimensions of the Desktop enclosure in its manual. The manual indicates a thickness of the Desktop enclosure's add-on card at about 1.4mm, which makes me think I'm getting the dimensions mixed up -- please correct me if I'm wrong. I couldn't find any dimensions for the aforementioned RPi HAT, but it's at most 50mm tall which only gives me about 41.72 mm of room, assuming my calculations are correct. So,it may or may not fit...

 

Thanks,

 

jdb2

  • Sign in to reply
  • Cancel
Parents
  • uscdadnyc
    0 uscdadnyc over 9 years ago

    To JB:  I have the same Q (sort of). [I do not have a e14-desktop yet either]  AAR does the e14-desktop use of the GPIO pins for their GPIO => mSATA=> mSATA SSD (up to 1TB), PRECLUDE Any Additional use of the GPIO pins?. Actually mSATA is a little antiquated (?), isn't there an m.2 Standard. I had an m.2 SSD in my Intel NUC5i7RYH, but it died. AAR my plans for an e14-desktop is to put an Up-board (SBC-Single Board Computer) inside. The Up-board has the same LxW dimensions as a RPi3B, but the H (Height) is a little larger. And instead of using the mSATA, I would try to expose/feed-back-in the USB-3.0-micro-B-connector on the Up-board AND(?) put a USB3.0 SSD (if there is such a Thing Yet). I already have Two WD PiDrives (HDDs) that are USB3.0, power consumption maybe too much for the e14-desktop. BTW1, I have an Up-board inside a Pi-TopCEED, running WIN10-64Pro. This Pi-TopCEED also accomodates my RPiZ's, RPiZW's as well as my Up-board. Of Course, One At A Time though. BTW2 My RPi3B is inside a SmartiPi Case, along w/ a 7" TouchScreen. I have posted on other e14 community discussion post(s) on how to Free the HDMI port that is Blocked on the SmartiPi Case. If you do purchase e14-desktop, please post Pictures of the inside. Thx.

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • uscdadnyc
    0 uscdadnyc over 9 years ago

    To JB:  I have the same Q (sort of). [I do not have a e14-desktop yet either]  AAR does the e14-desktop use of the GPIO pins for their GPIO => mSATA=> mSATA SSD (up to 1TB), PRECLUDE Any Additional use of the GPIO pins?. Actually mSATA is a little antiquated (?), isn't there an m.2 Standard. I had an m.2 SSD in my Intel NUC5i7RYH, but it died. AAR my plans for an e14-desktop is to put an Up-board (SBC-Single Board Computer) inside. The Up-board has the same LxW dimensions as a RPi3B, but the H (Height) is a little larger. And instead of using the mSATA, I would try to expose/feed-back-in the USB-3.0-micro-B-connector on the Up-board AND(?) put a USB3.0 SSD (if there is such a Thing Yet). I already have Two WD PiDrives (HDDs) that are USB3.0, power consumption maybe too much for the e14-desktop. BTW1, I have an Up-board inside a Pi-TopCEED, running WIN10-64Pro. This Pi-TopCEED also accomodates my RPiZ's, RPiZW's as well as my Up-board. Of Course, One At A Time though. BTW2 My RPi3B is inside a SmartiPi Case, along w/ a 7" TouchScreen. I have posted on other e14 community discussion post(s) on how to Free the HDMI port that is Blocked on the SmartiPi Case. If you do purchase e14-desktop, please post Pictures of the inside. Thx.

    USCDADNYC (NY NY USA)