Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Is the element14 Desktop enclosure compatible with GPIO add-on cards?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 707 subscribers
  • Views 1066 views
  • Users 0 members are here
  • ups
  • gpio
  • ups-pico
  • add-on-board
  • raspberry_pi
  • pi desktop
Related

Is the element14 Desktop enclosure compatible with GPIO add-on cards?

jdb2
jdb2 over 9 years ago

Hello. I've been thinking of getting an Element14 Raspberry Pi Desktop enclosure for my RPi 3, but, I need to know if the enclosure is compatible with the UPS-Pico GPIO add-on board ( UPS PIco HV3.0A Stack Plus with 450mAh Battery  ). I've called Newark/element14 tech support, but the support rep didn't have a definitive answer as even he couldn't find any dimensions for the Desktop enclosure.

 

Any help regarding this topic or how to possibly get around the space constraints, if possible, would be greatly appreciated.

 

EDIT : Stupid oversight on my part -- I missed the dimensions of the Desktop enclosure in its manual. The manual indicates a thickness of the Desktop enclosure's add-on card at about 1.4mm, which makes me think I'm getting the dimensions mixed up -- please correct me if I'm wrong. I couldn't find any dimensions for the aforementioned RPi HAT, but it's at most 50mm tall which only gives me about 41.72 mm of room, assuming my calculations are correct. So,it may or may not fit...

 

Thanks,

 

jdb2

  • Sign in to reply
  • Cancel
Parents
  • chris_b2b
    0 chris_b2b over 9 years ago

    The Pi Desktop board uses a loopback USB2 connector for the SATA functionality so no GPIO's are used for that.

    Since my project uses SPI & some GPIO pins i mapped them out, maybe it's useful to others too.

    The onboard MCU consumes i2c, SPI, UART and GPIO's 6, 13,19 & 26.

     

    Will have to see if CE1 (GPIO7) can still be used with an nRF24 device while this hat is on.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • chris_b2b
    0 chris_b2b over 9 years ago

    The Pi Desktop board uses a loopback USB2 connector for the SATA functionality so no GPIO's are used for that.

    Since my project uses SPI & some GPIO pins i mapped them out, maybe it's useful to others too.

    The onboard MCU consumes i2c, SPI, UART and GPIO's 6, 13,19 & 26.

     

    Will have to see if CE1 (GPIO7) can still be used with an nRF24 device while this hat is on.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • titou43
    0 titou43 over 8 years ago in reply to chris_b2b

    Hello

     

    I would like to mount this card on GPIO :

     

    https://shop.olmatic.de/en/ups-raspberry-pi/11-susv-pi-advanced-mobile-4260434190104.html

     

    It is a card for to pilot the power supply ....

    Is anyone could say me if this card function with the pi desktop ?

     

    I have look at the two manuals for the GPIO used :

     

    PI desktop :

    GPIO2

    GPIO3

    GPIO17

    GPIO6

    GPIO13

    GPIO19

    GPIO26

     

    Power Supply :

    + 5v (pin 2)

    GPIO2

    GPIO3

    GPIO27

    ID_SD (pin 27)

    ID_SC (pin 28)

     

    Many thanks