Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Capacitor to smooth out Raspberry Pi power dips?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 48 replies
  • Answers 30 answers
  • Subscribers 710 subscribers
  • Views 22378 views
  • Users 0 members are here
  • usb power
  • power supply
  • raspberry_pi
  • pi3
  • raspberry pi
  • usb cable
Related

Capacitor to smooth out Raspberry Pi power dips?

ntewinkel
ntewinkel over 9 years ago

I recently was trying to do a few things with a Pi3, and it consistently hung when I tried to update the system (sudo apt-get update/upgrade). It did everything else well enough, so I wonder if that's power related, with the upgrade making the WiFi work extra hard - maybe not, but I thought I'd look into it.

 

I've also noticed that my older Pi1 will hang once in a while (every few months), and that's a bit of an issue now that I'm using it as my sprinkler controller - reliability has become much more important.

 

While searching for help online, I noticed Robert Peter Oakes did some research and made a nice blog entry explaining the role the USB cables have in the power issues. (Thanks Peter!)

 

In a nutshell, some cables cause a voltage drop that puts the supply too far below the ideal 5v voltage level for the Pi.

The problem is that once in a while the Pi draws enough power to make the voltage dip into the danger zone.

(Some places sell adapters with a higher voltage to compensate. AdaFruit, for example sells a 5.25v adapter for the RPi, and notes that 5.25v is still within the specifications for USB, so even with a perfect no-loss USB cable that should be safe.)

 

One notable item, to me, was that the Pi has some serious power dips on a regular basis, regardless of the cables - just that the better supplies+cables start with higher levels at the Pi and the dips don't take it down too far.

 

So here's my thought - capacitors are supposed to help against dips and spikes, right?

 

Is there a way to add some really big capacitor at the Pi side to help avoid such dips (and maybe spikes too) ?

 

I'm thinking VIN-GND with a 1,000+ uF cap? I have one rated 1,000 at 10v, also I see 1,800 at 16v, both should handle 5v-ish well.

 

Otherwise, maybe splice a USB cable to add the large cap near the micro-USB plug end?

 

Will that cause trouble? Will it help at all?

 

Thanks!

-Nico

  • Sign in to reply
  • Cancel
Parents
  • mcb1
    0 mcb1 over 9 years ago

    I'm thinking VIN-GND with a 1,000+ uF cap

    The rule of thumb for filter capacitors is 1,000 uf per amp as the absolute minimum.

    This assumes the load is constant, but for your power dip issue, you really need to be looking at 10-20,000uF to be sure.

    You can try the other values and stick it across the 5v on the GPIO pins.

     

    You should be able to measure the 5v lines to see what you are actually getting.

    The GPIO is probably a good and easy place to get to.

     

     

    IMO most of the issues are the power supply themselves.

    I've run them from 700mA Samsung chargers with tiny leads while other 'genuine' supplies were below 5v.

    Most of the 'chargers' are simply a device to provide 5 ish volts to a phone to charge a 3.6v lithium battery, and were never designed to be a stable smooth 5.x volt power supply.

     

    You could have a mains issue, but with a switchmode supply (as most are nowdays) it should handle it.

     

     

    I don't suppose it's some dodgy software hobbled together by someone in some small backwater town ... image

    Mark

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 9 years ago in reply to mcb1

    >I don't suppose it's some dodgy software hobbled together by someone in some small backwater town ...

     

    Nah that stuff is solid!

    (the sprinkler controller is actually not my work - it's OpenSprinkler.com, but the kitty-cam.. that kitty-cam is solid like a rock!)

     

    The hanging was happening on a Pi3 with the latest Raspbian image just freshly copied to it (redid that again to make sure).

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 9 years ago in reply to mcb1

    >I don't suppose it's some dodgy software hobbled together by someone in some small backwater town ...

     

    Nah that stuff is solid!

    (the sprinkler controller is actually not my work - it's OpenSprinkler.com, but the kitty-cam.. that kitty-cam is solid like a rock!)

     

    The hanging was happening on a Pi3 with the latest Raspbian image just freshly copied to it (redid that again to make sure).