Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Capacitor to smooth out Raspberry Pi power dips?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 48 replies
  • Answers 30 answers
  • Subscribers 710 subscribers
  • Views 22314 views
  • Users 0 members are here
  • usb power
  • power supply
  • raspberry_pi
  • pi3
  • raspberry pi
  • usb cable
Related

Capacitor to smooth out Raspberry Pi power dips?

ntewinkel
ntewinkel over 9 years ago

I recently was trying to do a few things with a Pi3, and it consistently hung when I tried to update the system (sudo apt-get update/upgrade). It did everything else well enough, so I wonder if that's power related, with the upgrade making the WiFi work extra hard - maybe not, but I thought I'd look into it.

 

I've also noticed that my older Pi1 will hang once in a while (every few months), and that's a bit of an issue now that I'm using it as my sprinkler controller - reliability has become much more important.

 

While searching for help online, I noticed Robert Peter Oakes did some research and made a nice blog entry explaining the role the USB cables have in the power issues. (Thanks Peter!)

 

In a nutshell, some cables cause a voltage drop that puts the supply too far below the ideal 5v voltage level for the Pi.

The problem is that once in a while the Pi draws enough power to make the voltage dip into the danger zone.

(Some places sell adapters with a higher voltage to compensate. AdaFruit, for example sells a 5.25v adapter for the RPi, and notes that 5.25v is still within the specifications for USB, so even with a perfect no-loss USB cable that should be safe.)

 

One notable item, to me, was that the Pi has some serious power dips on a regular basis, regardless of the cables - just that the better supplies+cables start with higher levels at the Pi and the dips don't take it down too far.

 

So here's my thought - capacitors are supposed to help against dips and spikes, right?

 

Is there a way to add some really big capacitor at the Pi side to help avoid such dips (and maybe spikes too) ?

 

I'm thinking VIN-GND with a 1,000+ uF cap? I have one rated 1,000 at 10v, also I see 1,800 at 16v, both should handle 5v-ish well.

 

Otherwise, maybe splice a USB cable to add the large cap near the micro-USB plug end?

 

Will that cause trouble? Will it help at all?

 

Thanks!

-Nico

  • Sign in to reply
  • Cancel
Parents
  • ntewinkel
    0 ntewinkel over 9 years ago

    Here's an update...

     

    I received one of the new power adapters a few days ago and tried it last night.

    It's a Keyestudio 5.25v / 2.4A "highly regulated switching power supply". The first feature it mentions is compatibility with Raspberry Pi requirements. It's intended as a proper power supply - the cable is directly attached, and it says the wires are 20awg.

     

    I put my multimeter on 5v and GND and saw that at startup it was at exactly 5.25v, which then goes to about 5.20v while running, and down to about 5.16v while doing work.

    This is at multimeter display refresh, so there may be quick details I can't see without an oscilloscope of course.

     

    The point is that I no longer see the power-warning lightning bolt, and the WiFi connection appears to be much more stable - although it did disconnect once still during testing.

     

    Also, it wasn't my SD card as I first thought - I was able to run the updates for both SD cards I tried it with.

     

    So I think the lesson here is to use proper power supplies, not chargers (as so many people have said so many times!).

     

    And the other part of the lesson is to not blame the power supply for everything - in my case the dropped WiFi was causing my troubles, because due to it being a remote-desktop connection it became inaccessible, making it look like it was hanging.

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 9 years ago in reply to ntewinkel

    Another update, in case people are curious...

     

    My sprinkler Pi2 went unresponsive again on the weekend (last reset was 2 weeks earlier), so I decided that was a good time to switch power supplies for it - I had been using a 5v 2A tablet charger, so I now have it on the aforementioned Keyestudio power adapter.

     

    I then took the tablet power supply and put it on my Pi1 cat-video system (it plays videos for cats, LOL yes). It right away showed the coloured block at the top right indicating poor power supply.... hmmm interesting!

     

    So for the Pi1 I went back to a 2-usb-port charger supply (a cheap eBay one) that I'd been using for it, and the video flickers constantly, sometimes even keeping a blank screen - but no power-warning icon. So that video flicker issue I was trying to fix by changing config settings appears to be due to the poor power supply too. (ps, it's an old monitor with HDMI-to-DVI adapter)

     

    I have a different power adapter still on the way, but it's taking the scenic route. I'm curious as to how it will perform.

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 8 years ago in reply to ntewinkel

    Another update - the Sprinkler-Pi has been running reliably since the previous update, with the Keyestudio power adapter.

     

    The other adapter (5v, 3A) came in a few weeks ago and the kitty-tv Pi seems to be happy running on it - no power warnings, no flickering on/off video. (I haven't run this Pi a lot though).

     

    So it does seem that my problems were related to power, and the lesson I'm walking away with is that Raspberry Pis should be powered by purpose-built power adapters, not cellphone or tablet chargers.

     

    -Nico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 8 years ago in reply to ntewinkel

    Another update - the Sprinkler-Pi has been running reliably since the previous update, with the Keyestudio power adapter.

     

    The other adapter (5v, 3A) came in a few weeks ago and the kitty-tv Pi seems to be happy running on it - no power warnings, no flickering on/off video. (I haven't run this Pi a lot though).

     

    So it does seem that my problems were related to power, and the lesson I'm walking away with is that Raspberry Pis should be powered by purpose-built power adapters, not cellphone or tablet chargers.

     

    -Nico