Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Capacitor to smooth out Raspberry Pi power dips?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 48 replies
  • Answers 30 answers
  • Subscribers 710 subscribers
  • Views 22269 views
  • Users 0 members are here
  • usb power
  • power supply
  • raspberry_pi
  • pi3
  • raspberry pi
  • usb cable
Related

Capacitor to smooth out Raspberry Pi power dips?

ntewinkel
ntewinkel over 9 years ago

I recently was trying to do a few things with a Pi3, and it consistently hung when I tried to update the system (sudo apt-get update/upgrade). It did everything else well enough, so I wonder if that's power related, with the upgrade making the WiFi work extra hard - maybe not, but I thought I'd look into it.

 

I've also noticed that my older Pi1 will hang once in a while (every few months), and that's a bit of an issue now that I'm using it as my sprinkler controller - reliability has become much more important.

 

While searching for help online, I noticed Robert Peter Oakes did some research and made a nice blog entry explaining the role the USB cables have in the power issues. (Thanks Peter!)

 

In a nutshell, some cables cause a voltage drop that puts the supply too far below the ideal 5v voltage level for the Pi.

The problem is that once in a while the Pi draws enough power to make the voltage dip into the danger zone.

(Some places sell adapters with a higher voltage to compensate. AdaFruit, for example sells a 5.25v adapter for the RPi, and notes that 5.25v is still within the specifications for USB, so even with a perfect no-loss USB cable that should be safe.)

 

One notable item, to me, was that the Pi has some serious power dips on a regular basis, regardless of the cables - just that the better supplies+cables start with higher levels at the Pi and the dips don't take it down too far.

 

So here's my thought - capacitors are supposed to help against dips and spikes, right?

 

Is there a way to add some really big capacitor at the Pi side to help avoid such dips (and maybe spikes too) ?

 

I'm thinking VIN-GND with a 1,000+ uF cap? I have one rated 1,000 at 10v, also I see 1,800 at 16v, both should handle 5v-ish well.

 

Otherwise, maybe splice a USB cable to add the large cap near the micro-USB plug end?

 

Will that cause trouble? Will it help at all?

 

Thanks!

-Nico

  • Sign in to reply
  • Cancel
Parents
  • fvan
    0 fvan over 9 years ago

    Those power dips sound strange!

     

    I'm able to run a Pi 3 with official touch screen on a single 5.1V/2.5A official power supply. Occasionally the little lightning symbol pops up, but certainly no hanging.

     

    What are the specs of your power supply? Have you tried another?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 9 years ago in reply to fvan

    Thanks Frederick,

     

    >What are the specs of your power supply? Have you tried another?

    I tried a few, including a Samsung 5V2A charger for my Nexus 10, and an Apple iPad (2) charger. And then I saw Peter's post about cables often being the issue - my testing then confirmed that to be true, so I picked out the better cables I have, and ordered some adapters with the higher starting voltage (5.25v) to compensate for cable losses. I also bought some USB ends to solder up my own (power-only) cables using some larger gauge wires to see if that helps.

     

    My question was more about the dips at the Pi end being a concern.

     

    (my Pi1 sprinkler controller has a charger from a 7" Android tablet, not sure of the specs but it's behaved well for the most part)

     

    Thanks,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 9 years ago in reply to ntewinkel

    My question was more about the dips at the Pi end being a concern.

    Well.... The pi will boot (which seems to be a bit more demanding in my testing) fine with the voltage at the pi being 2.8V or 2.9V. It kept running down to a few hundred mV less, as long as it had completed the boot process.

     

    So for the pi to crash you need pretty serious dips....

     

    If you say your cable is OK, then the pi is simply pulling the powersupply into an overcurrent condition or something like that.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • rew
    0 rew over 9 years ago in reply to ntewinkel

    My question was more about the dips at the Pi end being a concern.

    Well.... The pi will boot (which seems to be a bit more demanding in my testing) fine with the voltage at the pi being 2.8V or 2.9V. It kept running down to a few hundred mV less, as long as it had completed the boot process.

     

    So for the pi to crash you need pretty serious dips....

     

    If you say your cable is OK, then the pi is simply pulling the powersupply into an overcurrent condition or something like that.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer