Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Nintendo Pi Zero (NPZ) Project Help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 705 subscribers
  • Views 828 views
  • Users 0 members are here
  • raspberry_pi
Related

Nintendo Pi Zero (NPZ) Project Help

rivera82falcon
rivera82falcon over 8 years ago

As in the title, I'm working on a project with my son making an NES using the Raspberry Pi Zero and integrating it into a Retro Entertainment System. https://i.imgur.com/WkQh28f.jpg

 

I've opened it up (https://i.imgur.com/nyhAM9d.jpg) and it looks simple enough to remove anything "useless" and get the Zero inside. I want to keep the controller board so I traced everything out (https://i.imgur.com/nNmjFIj.jpg), desoldered the old cable and applied pins in its place for easy cable swapping/testing (https://i.imgur.com/6RoGdN7.jpg). I have everything layed out (https://i.imgur.com/GUeKnCi.jpg) and just about complete. I want to also use the power/reset from the controller board but this is where I'm lost.

 

From the pinout I traced, P11 would be Power, P12 would be Negative I believe for Power and Reset, and P2 is positive for Reset (if someone doesn't mind checking my work I would be very greatful https://i.imgur.com/hnWczuj.jpg (top is P1)). Again, at this part, I'm lost and could use a little nudge in the right direction being that this is my first project using a Pi. One last question: how do I know the Pi is running w/o the video plugged in? Is there an LED that needs a working image to run or will it turn on regardless if a micro SD card is installed? Thank you all for the support!!!

 

Edit: Not sure why but when I checked my links out, nNmjFLj.jpg comes up as removed but manually typing it in the address bar works. Not sure if others are gonna see that.

  • Sign in to reply
  • Cancel
Parents
  • rivera82falcon
    0 rivera82falcon over 8 years ago

    Well, a little update on this. I'm going to be tackling the power surely, however I have been able to answer some of my own questions. I have the Raspberry Pi working, after finding a bad SD card. I have the controller working using the NES Port as well. One thing I did find out is that depending on what controller I am using I may have to swap out the data 1 pin and the clock pin. I might later on down the road rig up some switch in the event I have to use a different controller that would require those two pins to be swapped however at this time it's not a major issue. I will post some pictures after I finish doing some errands but I'm happy that this is off to a great start after doing trial and errors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rivera82falcon
    0 rivera82falcon over 8 years ago

    Well, a little update on this. I'm going to be tackling the power surely, however I have been able to answer some of my own questions. I have the Raspberry Pi working, after finding a bad SD card. I have the controller working using the NES Port as well. One thing I did find out is that depending on what controller I am using I may have to swap out the data 1 pin and the clock pin. I might later on down the road rig up some switch in the event I have to use a different controller that would require those two pins to be swapped however at this time it's not a major issue. I will post some pictures after I finish doing some errands but I'm happy that this is off to a great start after doing trial and errors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • rivera82falcon
    0 rivera82falcon over 8 years ago in reply to rivera82falcon

    https://i.imgur.com/r5HY8n1.jpg

    https://i.imgur.com/DTqNCdn.jpg

     

    This is the setup I am using for my project. I have not taken a picture yet but I'm using pain two on the controller board and running that to the pi. That is giving me a perfectly working reset button. I am trying to figure out how to get the second controller working but have not been successful. I can get the pi to acknowledge two controllers but I cannot configure it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rivera82falcon
    0 rivera82falcon over 8 years ago in reply to rivera82falcon

    I finally got the controllers working, power switch good, reset working, and a complete project. I'll do my own write-up soon but I was able to research and figure out the issues. This topic can be closed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer