Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Problem with Pi Desktop Case
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 708 subscribers
  • Views 1747 views
  • Users 0 members are here
  • raspberry_pi_space
Related

Problem with Pi Desktop Case

joerg_reuter
joerg_reuter over 8 years ago

have the same problem as Robert (Pi Desktop very disappointing ). I have the Pi Desktop already a couple of weeks. At the beginning, everything went perfectly normal and suddenly I had no HDMI signal. Only through the tests of Robert I noticed that it really depends on the SD card. I have tried several SD cards with always the same result: If I start the device without extension everything works always problem-free. With extension, there is no HDMI signal when I press the normal power button. I turn off again (and do not pull the power supply!) And remove the SD card and insert it again, the system boots completely normal. I have a 128 GB Samsung SD card (the effect also occurs at 32 and 16 GB) and a Kingstion 120 GB SSD disk. The effect occurs with and without an SSD disk.

 

Video: https://youtu.be/Hv7WsLgQZJ8

  • Sign in to reply
  • Cancel
Parents
  • lincon_m
    0 lincon_m over 7 years ago

    Any solutions? I'm having the same problem! I bought just for the fancy case as the msata it's a terrible solution, i was expecting to connect a simple HD or SSD inside. But, I can't even use just the case because the power connection needs the ellement 14 board. and if I use it the video doesn't work.

    Thanks

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • lincon_m
    0 lincon_m over 7 years ago

    Any solutions? I'm having the same problem! I bought just for the fancy case as the msata it's a terrible solution, i was expecting to connect a simple HD or SSD inside. But, I can't even use just the case because the power connection needs the ellement 14 board. and if I use it the video doesn't work.

    Thanks