Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum under voltage detection - Raspberry Pi 3 B+
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 32 replies
  • Answers 26 answers
  • Subscribers 709 subscribers
  • Views 32884 views
  • Users 0 members are here
Related

under voltage detection - Raspberry Pi 3 B+

y2010x
y2010x over 8 years ago

There seems to be a serious issue with the power regulator on the Raspberry Pi 3 B+, e.g.: I tried the recommended power supply, but the Pi still indicates that under voltage detected, and it keeps failing (not able to initiate anything, e.g.: sudo raspi-config, sudo apt-get update, etc.)

 

I bought another power supply with 5V, 3A rating, and the issues remain the same!

 

Can you recommend a method that I can overcome such issue(s)? Please kindly advise. Thank you.

  • Sign in to reply
  • Cancel
Parents
  • keillrandor
    0 keillrandor over 8 years ago

    I have a PI 3B +, had similar under voltage warnings, both in Debian Stretch syslog and yellow flash icon on my connected official 7" screen (I don't use any GPIO voltage bridging). I use an iFi power 2.5A rated switching PSU with micro usb connected to the PI. I also fed the screen with another separate micro usb power source. With this setup I had voltage underruns every now and then during the boot sequence.

     

    PI<----angled micro USB cable/USB-A male 0.5m---> <----micro iFi USB female A adapter/DC pin cable 0.1m---> <--DC PIN cable to iFi PSU 1.5m? ---> wall DC 230V/50Hz

     

    I resorted to solder the angled micro USB connector to the DC-pin adapter, removing about 0.5 meter of cabling and a possibly weak USB A female adapter used above.

    It resolved the issue. It would have been interesting to use an oscilloscope, which I don't have, to monitor the improved voltage stability.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • keillrandor
    0 keillrandor over 8 years ago

    I have a PI 3B +, had similar under voltage warnings, both in Debian Stretch syslog and yellow flash icon on my connected official 7" screen (I don't use any GPIO voltage bridging). I use an iFi power 2.5A rated switching PSU with micro usb connected to the PI. I also fed the screen with another separate micro usb power source. With this setup I had voltage underruns every now and then during the boot sequence.

     

    PI<----angled micro USB cable/USB-A male 0.5m---> <----micro iFi USB female A adapter/DC pin cable 0.1m---> <--DC PIN cable to iFi PSU 1.5m? ---> wall DC 230V/50Hz

     

    I resorted to solder the angled micro USB connector to the DC-pin adapter, removing about 0.5 meter of cabling and a possibly weak USB A female adapter used above.

    It resolved the issue. It would have been interesting to use an oscilloscope, which I don't have, to monitor the improved voltage stability.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
No Data