Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum under voltage detection - Raspberry Pi 3 B+
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 32 replies
  • Answers 26 answers
  • Subscribers 701 subscribers
  • Views 31651 views
  • Users 0 members are here
Related

under voltage detection - Raspberry Pi 3 B+

y2010x
y2010x over 7 years ago

There seems to be a serious issue with the power regulator on the Raspberry Pi 3 B+, e.g.: I tried the recommended power supply, but the Pi still indicates that under voltage detected, and it keeps failing (not able to initiate anything, e.g.: sudo raspi-config, sudo apt-get update, etc.)

 

I bought another power supply with 5V, 3A rating, and the issues remain the same!

 

Can you recommend a method that I can overcome such issue(s)? Please kindly advise. Thank you.

  • Sign in to reply
  • Cancel
Parents
  • alinp
    0 alinp over 7 years ago

    I'm facing the same problem.

    At first I thought my switching PS was the culprit, but then I've switched to powering the Raspberry Pi 3B+ from a Rohde&Schwarz HMC8042 bench power supply which is more than capable of driving the Pi.
    Voltage was set to 5.1V.
    Current limit was set to 2.2A.

    According to the bench PS which shows real-time current consumption, the average (in my case, for the firmware I'm running (it's a RetroPie) it's around 600 mA. Even with this beefy bench power supply I still get the under-voltage warning. I've measured the voltage right at the USB input socket and it's 5.0V (so the cable drops 0.1V).
    If someone has an explanation for this, I'll be glad to hear it.
    I'm assuming it's either a bad LDO or a hardware design issue.









    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • luislabmo
    0 luislabmo over 7 years ago in reply to alinp

    The voltage drop may be caused by the USB cable used: length, cable thickness, connector quality (or specs) may be the most important factors to consider: see this comment and this one. In my Raspberry Pi Road Test I cover this in the Power Consumption section.

     

    The easiest way to discard a USB power problem with the Pi is to power it directly to the GPIO with a regulated power supply where you can reduce some risk factors by increasing the wire thickness, using connectors with a good current rating, etc. USB power issues are harder to troubleshoot as USB cables are sealed most of them without reliable specs available that will bring a lot of unknown factors -one of the main reasons why is good to have the official micro USB power supply for Raspberry Pimicro USB power supply for Raspberry Pi to discard USB power issues.

     

    Luis

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • luislabmo
    0 luislabmo over 7 years ago in reply to alinp

    The voltage drop may be caused by the USB cable used: length, cable thickness, connector quality (or specs) may be the most important factors to consider: see this comment and this one. In my Raspberry Pi Road Test I cover this in the Power Consumption section.

     

    The easiest way to discard a USB power problem with the Pi is to power it directly to the GPIO with a regulated power supply where you can reduce some risk factors by increasing the wire thickness, using connectors with a good current rating, etc. USB power issues are harder to troubleshoot as USB cables are sealed most of them without reliable specs available that will bring a lot of unknown factors -one of the main reasons why is good to have the official micro USB power supply for Raspberry Pimicro USB power supply for Raspberry Pi to discard USB power issues.

     

    Luis

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • alinp
    0 alinp over 7 years ago in reply to luislabmo

    As stated in my original issue

    I've measured the voltage right at the USB input socket and it's 5.0V (so the cable drops 0.1V).

    The measuring procedure was done using a MSOX3104TMSOX3104T oscilloscope with a passive 10:1 probe hooked up right to the power rail smoothing capacitor C84.
    *schematic from the official Rasberry Pi docs.

    Measuring on the oscilloscope (MSOX3104TMSOX3104T) was done using Roll mode, at a sampling rate of 100ms/division.
    At no point during the testing procedure, which involved throwing multiple power hungry tasks at the CPU, did the power supply (which again was a R&S HMC8042 OS) vary by more than 100mV. Overall, the voltage did no drop under 4.9V. Despite this, the low-voltage warnings kept coming. 

    The power was fed trough the USB port, using a high quality USB cable, that was cut to 5cm in order to expose the power and GND wires inside an hook them up to the bench PS.

    Given above testing procedure I can confidently exclude any factor related to the USB cable or power supply being used. Thus, I conclude that there must be a faulty hardware design somewhere down the line. If someone has identified it or has a different opinion please let me know.

    I still don't know if I should send in back to Farnell under warranty due to this malfunction.




    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer