Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum NOOB: Rasberry Pi or Arduino - Larson Bar controlled by smartphone bluetooth
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 707 subscribers
  • Views 780 views
  • Users 0 members are here
  • bluetooth
  • led
  • raspberry_pi
  • arduino
Related

NOOB: Rasberry Pi or Arduino - Larson Bar controlled by smartphone bluetooth

cburnett1981
cburnett1981 over 11 years ago

I realize that the following project is not a beginner project.  And I am a beginner.  However, before I spend $ and time w/ either Rasberry Pi or Arduino, I'd like some input.

 

My final objective (who knows when I'll get to it) would be to create:

  • a ~20-24" long,  Larson Scanner, with
  • variable intensity low, med, high strength LED
  • Variable speed
  • variable color RGB
  • all controlled by Android or iOS over bluetooth.
  • battery or a/c powered

 

Example of commercial product w/ additional features that I can do w/o (audio and tactile)

 

Example of Ardiuno project of larson scanner, but missing a few features, key:  bluetooth.  I'm considering using Blynk, but bluetooth isn't currently an available option  (Blynk site reports next generation).  Also looking at a kickstarter for LightBlue Bean+

 

As I have no preference for Arduino over Rasberry Pi, some of what I have read in researching this project is that Rasberry Pi may be easier for Droid/iOS integration (those articles may have been out of date).

 

Thanks,

Casey

www.emdrforathletes.com

  • Sign in to reply
  • Cancel
Parents
  • clem57
    clem57 over 11 years ago

    Hi,

         Although you have posted in Raspberry Pi, this would work well with Arduino. To add Bluetooth, add a shield for the Arduino like http://www.seeedstudio.com/wiki/Bluetooth_Shield

    In the second demo is the programming to connect to a phone and connect a temperature sensor. But you can ignore that part, since you will use to change the action of the LED's. The Raspberry route is doable with a bit more programming because of Linux things. Nice links btw. Please post what you do for the build. I am sure you can get any help you need here.

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • clem57
    clem57 over 11 years ago

    Hi,

         Although you have posted in Raspberry Pi, this would work well with Arduino. To add Bluetooth, add a shield for the Arduino like http://www.seeedstudio.com/wiki/Bluetooth_Shield

    In the second demo is the programming to connect to a phone and connect a temperature sensor. But you can ignore that part, since you will use to change the action of the LED's. The Raspberry route is doable with a bit more programming because of Linux things. Nice links btw. Please post what you do for the build. I am sure you can get any help you need here.

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • cburnett1981
    cburnett1981 over 11 years ago in reply to clem57

    Hi @Mention do you think I should repost in Arduino?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to cburnett1981

    cburnett1981

         No problem, just leave here until you decide and then you can edit to move it at the bottom.

    C