Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Digital input & Relay output card for Raspberry Pi 3 Model B
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 4 answers
  • Subscribers 709 subscribers
  • Views 1426 views
  • Users 0 members are here
  • rasberry_pi_3_b_plus
  • raspberry_pi
Related

Digital input & Relay output card for Raspberry Pi 3 Model B

jirafeprasanna
jirafeprasanna over 8 years ago

Hi

 

I am looking for Digital input & Relay output card for Raspberry Pi 3 Model B.

so help me which card will be compatible for this application.

 

by this card I want to interface Push Button input to Raspberry Pi & want to switch ON relay for further control.

for more detail you can refer attach file.

 

 

Thanks

Prasanna Jirafe

9922135365

 




   
 
 
 
 
 
 
 
 
 
 
 






   
 
 
 
 
 
 
 
 
 
 
 





Attachments:
imageRP.docx
  • Sign in to reply
  • Cancel
Parents
  • Sean_Miller
    0 Sean_Miller over 8 years ago

    You can make this.  You need a tactile switch, 10K pull-up resistor, an NPN transistor, 1K resistor between the Pi output and transistor gate, and a relay.  You can google the schematic.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mcb1
    0 mcb1 over 8 years ago in reply to Sean_Miller

    Even better use the opto-coupled relays and you might need to reduce the series resistor

     

    RELAYS and POWER CONTROL

    Read the note about reducing the series resistor when driving from the Raspberry Pi.

    NOTE: It is sometimes possible to use these relay boards with 3.3V signals, IF the JD-VCC(RelayPower) is provided from a +5V supply and the VCC to JD-VCC jumper is removed. . That 5V relay supply could be totally isolated from the 3.3V device, or have a common ground IF opto-isolation is not needed.  If used with isolated 3.3V signals, VCC (To the input of the opto-isolator, next to the IN pins) should be connected to the 3.3V device's +3.3V supply. NOTE: Some RaspberryPi users have found that some relays are reliable and others do not actuate sometimes. It may be necessary to change the value of R1 from 1000 ohms to something like 220 ohms, or supply +5V to the VCC connection.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 8 years ago in reply to Sean_Miller

    Even better use the opto-coupled relays and you might need to reduce the series resistor

     

    RELAYS and POWER CONTROL

    Read the note about reducing the series resistor when driving from the Raspberry Pi.

    NOTE: It is sometimes possible to use these relay boards with 3.3V signals, IF the JD-VCC(RelayPower) is provided from a +5V supply and the VCC to JD-VCC jumper is removed. . That 5V relay supply could be totally isolated from the 3.3V device, or have a common ground IF opto-isolation is not needed.  If used with isolated 3.3V signals, VCC (To the input of the opto-isolator, next to the IN pins) should be connected to the 3.3V device's +3.3V supply. NOTE: Some RaspberryPi users have found that some relays are reliable and others do not actuate sometimes. It may be necessary to change the value of R1 from 1000 ohms to something like 220 ohms, or supply +5V to the VCC connection.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer