Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum A File Server That Won't Share Shares
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 11 answers
  • Subscribers 708 subscribers
  • Views 4041 views
  • Users 0 members are here
  • raspberry_pi
Related

A File Server That Won't Share Shares

oghma
oghma over 8 years ago

I've moved on from my first post "What Are The Basics?"

 

For context, my HW:

Raspberry Pi 3 B+ and a 16Gb mSD card with LITE imaged onto it

Pi-Desktop and a Kingston 480Gb mSATA

USB Keyboard/Mouse combo

10.1” TFT LCD Colour Monitor and a 20cm HDMI cable

 

For context, my environment::

Cat5e with RJ45 ports leading to a HP hub.

(Wi-Fi useless in my old house with thick walls. Not willing to spend a fortune with Wi-Fi extenders. Tried one - doesn't work well.)

What I've done:
used fstab to mount three partitions on the mSATA so they are there at bootup.
lines follow the format:

PARTUUID=5daf9610-09    /mnt/MYLABEL    vfat    defaults,auto,umask=000,users,rw 0 0

where 09 is either 01, 02 or 03 and MYLABEL are the three associated folders in /mnt that are my mountpoints.

 

When I issue a "mount" command I get:

/dev/sda9 on /mnt/MYLABEL type vfat (rw, nosuid,nodev,noexec,relatime,fmask=000,dmask=000,allow_utime=0022,codepage=437,iocharset=asci,shortname=mixed.errors=remount-ro)

where 9 is either 1, 2 or 3 and MYLABEL are the three associated folders in /mnt that are my mountpoints.

The options "nosuid, nodev and noexec" are unexpected, as I thought the opposite values are set by the "default" option.

 

I have confirmed that these mounts are owned by root.

 

I have updated the smb.conf with the following:

[global]

case sensitive = auto

preserve case = yes

short preserve case = yes

netbios name = Pi

server string = RaspFS01

workgroup = MYWKGRP

 

[MYSHARE9]

# share for the partition MYLABEL

path = /mnt/MYLABEL

comment = My sharing folders

browseable = yes

writeable = yes

only guest = no

create mask = 0777

directory mask = 0777

public=no

valid users = MYUSERS

force group = MYWKGRP

 

where 9 is 1, 2 or 3. MYLABEL is the same as the mountpoints above. MYUSERS is a comma seperated list of accounts I created including the user pi (See my next step). MYWKGRP is the workgroup I have on my PC.

 

I have set up users using "adduser" command

I have also made them members of the same groups as user pi

 

I have made the Pi boot with a static IP address and identified the static gateway and static_domain_name_servers as my BT Router.
Once rebooted I can ping google, so I'm still connected to the internet. I've also successfully run the update on the OS.
Now the fun!
When I try to create a mapping from my PC to the Pi, I get "Access Denied" no matter what user I use, even pi.
I ran the diagnostics from my PC and I can find the server, (although it does not show up in Networks). I even confirm the share exists. I just can't map to it.
I try to change the ownership of the mounts from root using the chmod command, but I get "Operation is not allowed". (Yes with sudo.)
I can't seem to allow any user to use these mounts remotely. I can only use them from the Pi! This is not a file server, but just a workstation. I can't find a way to associate MYWKGRP with these mounts with the right permissions.
I've seen a way to explicitly state a user and passwaord in the fstab file, but that would not syncronise with any change of password with the PC. (Not to mention the horrible hole in security!)
Can anyone tell me what I'm missing? Thanks for reading this far.
  • Sign in to reply
  • Cancel
Parents
  • jack.chaney56
    0 jack.chaney56 over 8 years ago

    I'd like to suggest checking out http://www.linuxfromscratch.org and checking out the Beyond Linux From Scratch section. In there (Section IV. Networking) it covers software and configuration for setting up SAMBA as well as several other server host options.

     

    Jack

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • oghma
    0 oghma over 8 years ago in reply to jack.chaney56

    Jack,

     

    This looks like the most comprehensive collection of actual configuration advice I've seen to-date. Thank you.

     

    I take your point that at this stage you are drawing my attention to particular sections, however, I feel that I should take a look at the whole journey to improve my understanding of how the parts of Linux work together. It's been far too long since I built servers, and I think the whole thing will do me some good. I plan to start with the first book before getting to the Beyond Linux From Scratch page(s). Of course, the only down side of this is that there are 370 pages in the first book alone!

     

    Thanks again. I'll let you know how I get on. (I'm a slow reader, so this could take a while.)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ebalem
    0 ebalem over 8 years ago in reply to oghma

    I've just seen your posts and the suggestions about share problems, and I wonder if the problem is with windows 10 not your pi server.

    In recent builds of win10 they have removed the homegroup support and do not by default include support for older versions of smb sharing.

    Simple workgroup sharing is now much more tricky even between windows pc's. It may be worth you searching on these issues to find more info.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • ebalem
    0 ebalem over 8 years ago in reply to oghma

    I've just seen your posts and the suggestions about share problems, and I wonder if the problem is with windows 10 not your pi server.

    In recent builds of win10 they have removed the homegroup support and do not by default include support for older versions of smb sharing.

    Simple workgroup sharing is now much more tricky even between windows pc's. It may be worth you searching on these issues to find more info.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • oghma
    0 oghma over 8 years ago in reply to ebalem

    Eddie,

     

    I was never using the <HOMEGROUP> feature. Also, as my nework is on the same subnet, I did not need to use a <DOMAIN>.

     

    I've checked that <MYWORKGROUP> is set for both the Pi and my PC. I can also see another Win10 PC on the same subnet, with the same <MYWORKGROUP>. The windows side would appear to be behaving itself!

     

    I keep coming back to the permissions or the mount parameters. I'm about half way through the big read from Jack's post. I'll keep you all posted with my progress. Thanks again for your advice.