Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum A File Server That Won't Share Shares
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 11 answers
  • Subscribers 708 subscribers
  • Views 4025 views
  • Users 0 members are here
  • raspberry_pi
Related

A File Server That Won't Share Shares

oghma
oghma over 8 years ago

I've moved on from my first post "What Are The Basics?"

 

For context, my HW:

Raspberry Pi 3 B+ and a 16Gb mSD card with LITE imaged onto it

Pi-Desktop and a Kingston 480Gb mSATA

USB Keyboard/Mouse combo

10.1” TFT LCD Colour Monitor and a 20cm HDMI cable

 

For context, my environment::

Cat5e with RJ45 ports leading to a HP hub.

(Wi-Fi useless in my old house with thick walls. Not willing to spend a fortune with Wi-Fi extenders. Tried one - doesn't work well.)

What I've done:
used fstab to mount three partitions on the mSATA so they are there at bootup.
lines follow the format:

PARTUUID=5daf9610-09    /mnt/MYLABEL    vfat    defaults,auto,umask=000,users,rw 0 0

where 09 is either 01, 02 or 03 and MYLABEL are the three associated folders in /mnt that are my mountpoints.

 

When I issue a "mount" command I get:

/dev/sda9 on /mnt/MYLABEL type vfat (rw, nosuid,nodev,noexec,relatime,fmask=000,dmask=000,allow_utime=0022,codepage=437,iocharset=asci,shortname=mixed.errors=remount-ro)

where 9 is either 1, 2 or 3 and MYLABEL are the three associated folders in /mnt that are my mountpoints.

The options "nosuid, nodev and noexec" are unexpected, as I thought the opposite values are set by the "default" option.

 

I have confirmed that these mounts are owned by root.

 

I have updated the smb.conf with the following:

[global]

case sensitive = auto

preserve case = yes

short preserve case = yes

netbios name = Pi

server string = RaspFS01

workgroup = MYWKGRP

 

[MYSHARE9]

# share for the partition MYLABEL

path = /mnt/MYLABEL

comment = My sharing folders

browseable = yes

writeable = yes

only guest = no

create mask = 0777

directory mask = 0777

public=no

valid users = MYUSERS

force group = MYWKGRP

 

where 9 is 1, 2 or 3. MYLABEL is the same as the mountpoints above. MYUSERS is a comma seperated list of accounts I created including the user pi (See my next step). MYWKGRP is the workgroup I have on my PC.

 

I have set up users using "adduser" command

I have also made them members of the same groups as user pi

 

I have made the Pi boot with a static IP address and identified the static gateway and static_domain_name_servers as my BT Router.
Once rebooted I can ping google, so I'm still connected to the internet. I've also successfully run the update on the OS.
Now the fun!
When I try to create a mapping from my PC to the Pi, I get "Access Denied" no matter what user I use, even pi.
I ran the diagnostics from my PC and I can find the server, (although it does not show up in Networks). I even confirm the share exists. I just can't map to it.
I try to change the ownership of the mounts from root using the chmod command, but I get "Operation is not allowed". (Yes with sudo.)
I can't seem to allow any user to use these mounts remotely. I can only use them from the Pi! This is not a file server, but just a workstation. I can't find a way to associate MYWKGRP with these mounts with the right permissions.
I've seen a way to explicitly state a user and passwaord in the fstab file, but that would not syncronise with any change of password with the PC. (Not to mention the horrible hole in security!)
Can anyone tell me what I'm missing? Thanks for reading this far.
  • Sign in to reply
  • Cancel
Parents
  • 14rhb
    0 14rhb over 8 years ago

    Steven,

     

    Useful reading material on NFS and file access - I think your anser can be found in there, especially if you set up NFS. image

     

    https://linuxconfig.org/how-to-configure-nfs-on-linux

     

    https://raspberrypi.stackexchange.com/questions/87057/cannot-automatically-mount-nfs-share-to-raspberry-pi

     

    https://serverfault.com/questions/212178/chown-on-a-mounted-nfs-partition-gives-operation-not-permitted

     

    The last link perhaps contains something really useful...

    "By default the root_squash export option is turned on, therefore NFS does not allow a root user from the client to perform operations as root on the server, instead mapping it to the user/group id specified by anonuid and anongid options (default=65534). This is configurable in /etc/exports together with other export options."

     

    Rod

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • oghma
    0 oghma over 8 years ago in reply to 14rhb

    14rhb,

    Thanks for the imput, but I only have one Linux machine - the Pi. Not going to migrate my entire collection of computers over-night, especially since I'm having these issues.

     

    shabaz,

     

    This was useful. I went back to my notes on what I did and realised that I did not modify the permissions on the /mnt/MYLABELS mount points. So...

     

    umount the three /MYLABELS

     

    ls -l gives:

    drwxr-xr-x 2 root root 4096 Jul 24 15:34 MYLABEL

    where MYLABEL is one of my three mount point folders. They are all the same.

     

    sudo chmod 777 /mnt/MYLABEL

    Did this for all three.

     

    sudo chgrp users *

    (I only have the three mount point folders in /mnt, so I changed all of them at once.)

     

    ls -l now gives:

    drwxrwxrwx 2 root users 4096 Jul 24 15:34 MYLABEL

    where MYLABEL is as above.

     

     

    Now I try to map from Windows 10.

     

    Network still doesn't show the Pi. However, I can ping either the IP or the HostName from my PC.

     

    When I use \\HostName\SHARENAME

    where SHARENAME is the section name in smb.conf, I can 'browse' and see all the shares.

     

    However, providing the credentials of my new user I get the same Access Denied message.

    Providing the credentials of the user pi I get the message 'The user name or password is incorrect'.

    Obviously I rechecked the passwords by logging in and out with both the user pi and my new user. Both worked.

     

     

    I seem to be creeping forward, but as you can imagine, this is very frustrating. There seems to be no central admin tool like there was in Novel. I'm sure I'm at the point where this behaviour is so unlikely that a solution is far from obvious. As I'm exhibiting more experience than the average newbie, I don't know if the assumption will be that I've done everything right, so the response will be, "Well, that's a poser!". I'm willing to check every step, again. But I'm currently out of ideas on where to look. Everything seems fine to me, except that it doesn't work. Thanks for reading this far.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • 14rhb
    0 14rhb over 8 years ago in reply to oghma

    Hi Steven,

     

    My apologies - I misread your post and thought you were trying to transfer between two Linux boxes....in which case you can ignore all of what I've said (unless you are bored and want a good read image ).

     

    The command lsblk and the utility gnome-disks are sometimes useful for seeing what is mounted/unmounted and where they reside. When I've had errors refusing access after mounting a usb pendrive I've also used sudo chown -hR <user><group> <path to drive> 

     

    regards,

     

    Rod

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • oghma
    0 oghma over 8 years ago in reply to 14rhb

    14rhb/Rod,

     

    The lsblk command shows what I expect. The sda name is split into my three partitions.

     

    The gnome-disks utility is for GUI, but I have a LITE installation. I'm deliberatly avoiding a GUI install to increate the available space for my Spooler, if I ever get that far!

     

    The chown command has now changed the owner, so ls -l now gives:

    drwxrwxrwx 2 pi users 4096 Jul 24 15:33 MYLABEL
    where MYLABEL are the three associated folders in /mnt that are my mountpoints.
    This has made no difference to the problem I have, as stated in my post after shabaz. I still can't map to the MYLABELs. Credentials on my user gives Access Denied, and pi credentials still give me a 'The user name or password is incorrect' message.
    I can't help be think that this is a permissions issue. However, I don't know how to make all the different areas match. Can someone give me pointers to check what where? Thanks for reading this far.
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 8 years ago in reply to oghma

    I'm wondering if the errors you're getting could be specific to the Windows versions. What is the precise text of the error messages?

    There are some error messages on XP described here:

    https://ask.fedoraproject.org/en/question/109910/samba-and-windows-xp-unknown-user-name-or-bad-password/

    However with Windows 10 which you mention you tried, it refers to a slightly different error that doesn't mention the username:

    https://superuser.com/questions/1125438/windows-10-password-error-with-samba-share

    Anyway it could be worth making the changes suggested in these links too, in case it helps.

    Unfortunately I've not tried this, so I can only suggest some vague ideas : (

    Sometimes I'll also try to do a packet capture to see how far the protocol got, but I don't know this protocol well enough to be sure if this is a good idea, or a useless idea.

    There could also possibly be error messages somewhere in /var/log on the pi (type ls -altr to see the latest modified files there as the last ones in the list).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 8 years ago in reply to oghma

    I'm wondering if the errors you're getting could be specific to the Windows versions. What is the precise text of the error messages?

    There are some error messages on XP described here:

    https://ask.fedoraproject.org/en/question/109910/samba-and-windows-xp-unknown-user-name-or-bad-password/

    However with Windows 10 which you mention you tried, it refers to a slightly different error that doesn't mention the username:

    https://superuser.com/questions/1125438/windows-10-password-error-with-samba-share

    Anyway it could be worth making the changes suggested in these links too, in case it helps.

    Unfortunately I've not tried this, so I can only suggest some vague ideas : (

    Sometimes I'll also try to do a packet capture to see how far the protocol got, but I don't know this protocol well enough to be sure if this is a good idea, or a useless idea.

    There could also possibly be error messages somewhere in /var/log on the pi (type ls -altr to see the latest modified files there as the last ones in the list).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • oghma
    0 oghma over 8 years ago in reply to shabaz

    shabaz,

     

    I am only using Windows 10. The second link has lead me on a trail to use make amendments to my smb.conf and the pdbedit utility. It turns out that I added the pi user to samba, but not the new user. D'oh!

     

    Not quite there yet, as I'm still getting an error message, all be it a different one. However, I did manage to map to the Pi, but not with one of my shares! I just have to figure out where it connects to and why, then I might make some progress. It's taken me all day, so I've not even begun on Sean's help yet.

     

    I'll keep you both posted on my progress and the new lines in smb.conf, when it's a bit more stable. Thanks guys so far.