Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum How do I connect a car TFT screen to a raspberry pi 2b
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 705 subscribers
  • Views 3191 views
  • Users 0 members are here
  • raspberry_pi_space
Related

How do I connect a car TFT screen to a raspberry pi 2b

wayne.t.johnson
wayne.t.johnson over 8 years ago

Let me start off by saying I am a noob at this stuff but a fast leaner.  This is something I have been wanting to do for a while which is to make a portable gaming device with a raspberry pi.  Now I have the raspberry pi but can not for the life of me figure out how to connect a TFT screen to it because the cables do not fit the pi itself.  I have 8 lcd's with with 4 of them having a removable touchscreen, and one portable Blu-ray player.  I  have looked really hard to find someone using theses types of screens but almost all of them are using ones with a red, white, and yellow cables.  I really want to use the Blu-ray player  because I can also use the case and the rechargeable battery pack which is another issue because it pumps out 7.2v and I am afraid that it might short out the pi.  Can anyone please help me with this?imageimageimage

  • Sign in to reply
  • Cancel
Parents
  • wayne.t.johnson
    0 wayne.t.johnson over 8 years ago

    No it does not have yellow,  red, and white cables.  It has a ribbon cable and a pink and white power cable.  The ribbon cable fits but the screen is from a car radio so I think it is a 9v screen.  I also have a DVD player with output only and no input.  So I am trying to figure out how to connect it to the pi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • wayne.t.johnson
    0 wayne.t.johnson over 8 years ago

    No it does not have yellow,  red, and white cables.  It has a ribbon cable and a pink and white power cable.  The ribbon cable fits but the screen is from a car radio so I think it is a 9v screen.  I also have a DVD player with output only and no input.  So I am trying to figure out how to connect it to the pi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 8 years ago in reply to wayne.t.johnson

    If the ribbon cable is a flat flex cable directly from the TFT, then that's near-impossible to use easily, because there are many different configurations of interface and connector, and it would become a game of luck trying to find some adaptor or controller card that definitely works, and costs less overall compared to just buying a new display that is already intended for the Pi.

    If the ribbon cable is from some circuit board, you may have some luck trying to trace connections - without a circuit diagram some detailed photo would be needed to see if this is possible.

    The DVD player has an output, but internally the TFT accepts input signals, so any chance of getting it connected involves opening the player - but it is unlikely to be easily usable, because there is no need for the player internals to have any accessible HDMI or composite signals.