Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Setting up 7" LCD TFT Display 1024*600 with RPi 3
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 3 answers
  • Subscribers 706 subscribers
  • Views 2640 views
  • Users 0 members are here
Related

Setting up 7" LCD TFT Display 1024*600 with RPi 3

afmishaq
afmishaq over 7 years ago

I just bought a 7" LCD TFT Display 1024*600 HDMI VGA Monitor Screen Kit for Raspberry Pi 3. It came with no documentation I generally know how to go about setting it up but I was wondering if someone has recently done it and could point me in th eright direction A picture of what I got is attached. I intend to use it with RPi 3 B+ and Rasbian Stretch.

 

The specs in the listing say it will require 12 V but the power cable supplied has USB connector at the other end! Guess, I can always try it with 5V. The other question is whether any edits are required to the config file?

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 7 years ago

    Hi Abul,

     

    I have something similar, although I don't really use it with the pi (because the display resolution was low for the one i had - but it was useful for non-Pi scenarios).

    It just works when connected, it likely sets itself up to match the resolution settings as best as it can manage, using the out-of-band channel that is over the HDMI connection. And the buttons could be used for tweaking settings or you may find no adjustment is needed at all. These displays should be handy for connecting to games systems (but regrettably my Nintendo doesn't have HDMI : ( or converting a Pi into a retro games system, there is a very huge thread on it here: PIK3A: The Raspberry Pi 3 IKEA Retro Gaming Table

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 7 years ago

    Hi Abul,

     

    I have something similar, although I don't really use it with the pi (because the display resolution was low for the one i had - but it was useful for non-Pi scenarios).

    It just works when connected, it likely sets itself up to match the resolution settings as best as it can manage, using the out-of-band channel that is over the HDMI connection. And the buttons could be used for tweaking settings or you may find no adjustment is needed at all. These displays should be handy for connecting to games systems (but regrettably my Nintendo doesn't have HDMI : ( or converting a Pi into a retro games system, there is a very huge thread on it here: PIK3A: The Raspberry Pi 3 IKEA Retro Gaming Table

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • afmishaq
    0 afmishaq over 7 years ago in reply to shabaz

    Hi Shabaz,

     

    Yes, and that is why it must be powered up before the device it is connecting. Since the processor in the display controller has a scaler, it can scale down a suitable higher resolution that best fits it pixel geometry.

     

    Thanks,

    - Faiz