Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Setting up 7" LCD TFT Display 1024*600 with RPi 3
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 3 answers
  • Subscribers 706 subscribers
  • Views 2642 views
  • Users 0 members are here
Related

Setting up 7" LCD TFT Display 1024*600 with RPi 3

afmishaq
afmishaq over 7 years ago

I just bought a 7" LCD TFT Display 1024*600 HDMI VGA Monitor Screen Kit for Raspberry Pi 3. It came with no documentation I generally know how to go about setting it up but I was wondering if someone has recently done it and could point me in th eright direction A picture of what I got is attached. I intend to use it with RPi 3 B+ and Rasbian Stretch.

 

The specs in the listing say it will require 12 V but the power cable supplied has USB connector at the other end! Guess, I can always try it with 5V. The other question is whether any edits are required to the config file?

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • korn
    0 korn over 7 years ago

    Looks a lot like the one I got from Adafruit except they dont have the remote.

     

    worked fine with a windows 10PC. With the PI you may have to tweak the config a bit.

     

    One thing I found is make sure the screen is powered up Before the PI.

     

    If the Pi boots first it goes into the wrong resolution.

     

    You may just have to change the boot file options for HDMI to force what settings you want then boot order wont matter

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • korn
    0 korn over 7 years ago

    Looks a lot like the one I got from Adafruit except they dont have the remote.

     

    worked fine with a windows 10PC. With the PI you may have to tweak the config a bit.

     

    One thing I found is make sure the screen is powered up Before the PI.

     

    If the Pi boots first it goes into the wrong resolution.

     

    You may just have to change the boot file options for HDMI to force what settings you want then boot order wont matter

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • afmishaq
    0 afmishaq over 7 years ago in reply to korn

    Robert,

     

    Thank you. That is a very useful tip, having the screen powered up before the pi.

     

    - Faiz