Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum What is the minimun supply voltage for the pi3b plus.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 6 answers
  • Subscribers 667 subscribers
  • Views 5130 views
  • Users 0 members are here
Related

What is the minimun supply voltage for the pi3b plus.

bjurg
bjurg over 6 years ago

What is the minimun voltage for the pi3b plus to prevent undervoltage. 4.98 V is observed to be too low, 5.1 V to be sufficient. With 4.98V undervoltage warnings exist and the processor seems to run approx half as fast.

  • Sign in to reply
  • Cancel
Parents
  • ralphjy
    0 ralphjy over 6 years ago

    It sounds like you are measuring at the source rather than on the RPi itself.  You might be having voltage drop in the power supply cable.  You should measure the voltage at the GPIO connector.  If those are voltages are measured at the at the GPIO connector then you need to look at the voltage on a scope to see whether you see lots of ripple or supply droop when running.  It would be good to measure the supply current also.  You could have a bad cable or possibly a bad RPi.  I've seen a lot of bad cables.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • gdstew
    0 gdstew over 6 years ago in reply to ralphjy

    Most "standard" USB cables are unsuitable for use as power cable for the Raspberry Pi. They usually use 28 AWG wire for the data signals and 26 AWG wire (lower AWG number is larger

    diameter wire) for power although I have also seen 28 AWG used for both. 26 AWG wire for power is way too small for the 2.5 A current needed by the Pi. 22 - 20 AWG should be used

    and I like to keep the cables lengths at 4 - 6 ft. (1.2 to 1.8m) max. Most USB cables, in the US at least, have markings that show the wire gauges used. The markings are usually in the form

    of 28AWG/2C+26AWG/2C which says that 2 wires are 28 gauge and 2 wires are 26 gauge. The lower AWG wires should always be the ones used for power. You can find USB cables with

    22 - 20 AWG power wires, usually specifically described as Pi power cables but you have to look a little harder for them. And of course the descriptions are not always accurate so buying

    from trusted sources helps. Being able to visually verify the gauge markings on the cables before purchase is best. I have been able on occasion to use advertisement pictures of the cables

    to read these markings but it is usually very difficult to be sure.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • luislabmo
    0 luislabmo over 6 years ago in reply to gdstew

    Add on top of that the ones that advertise thick wires and still won't work properly image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • luislabmo
    0 luislabmo over 6 years ago in reply to gdstew

    Add on top of that the ones that advertise thick wires and still won't work properly image