• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Raspberry Pi Forum Can Rpi read mass flow meter ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 9 answers
  • Subscribers 705 subscribers
  • Views 4031 views
  • Users 0 members are here
  • raspberry_pi
Related

Can Rpi read mass flow meter ?

netromaster
netromaster over 7 years ago

I am considering purchasing a coriolis mass flow meter that emits pulses for a project. I know it is quite common to read volumetric flow meters with the pi but I cannot say the same for the mass flow meter.

Now my question is this; if I purchase the coriolis meter, will I be able to hook it up to the pi as easy as the common flow meter and write code to determine flow rate and volume ?

  • Sign in to reply
  • Cancel
Parents
  • Problemchild
    0 Problemchild over 7 years ago

    Is this this an automotive MAF sensor?  As I remember many of those are a resistor bridge with one arm in the Air flow, in that case it's a process of measurement of how out of balance the bridge becomes and that's an analog problem.

    If you want to ensure you can read Pulses/Pulse rates or analog voltages at a fixed reliable rate I would consider using one of a million controllers  then offering it up  to the PI  for high level processing since you wouldn't need to worry about Linux latency issues presuming they are even an issue with your solution!

     

    Answer is yes but you'll need to elaborate on what you are doing !

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • netromaster
    0 netromaster over 7 years ago in reply to Problemchild

    It is not an automotive MAF sensor. It is a double tube coriolis meter for basically water and oil measurements. It does have a local interface showing massflow and volume readings. I plan to extend its features with my own controller to help me remotely get readings. Basically making it IoT complaint. Its is a generic flow meter with no claims on it.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mp2100
    0 mp2100 over 7 years ago in reply to netromaster

    As John said, the short answer is yes.  But whether the rPi is the best solution is a follow-up discussion.  Does the manufacturer tell you how fast the pulses are generated at normal flow?  The rPi is a Linux computer, so if pulses come very fast, it may be busy doing other Linux operating system things when it should be counting pulses.  A simpler microprocessor could be better for this than the rPi.

     

    An alternate route could be, if the coriolis meter supports modbus, there are modbus libraries for the rPi.  You'd use the UART serial pins to talk Modbus.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mp2100
    0 mp2100 over 7 years ago in reply to netromaster

    As John said, the short answer is yes.  But whether the rPi is the best solution is a follow-up discussion.  Does the manufacturer tell you how fast the pulses are generated at normal flow?  The rPi is a Linux computer, so if pulses come very fast, it may be busy doing other Linux operating system things when it should be counting pulses.  A simpler microprocessor could be better for this than the rPi.

     

    An alternate route could be, if the coriolis meter supports modbus, there are modbus libraries for the rPi.  You'd use the UART serial pins to talk Modbus.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • netromaster
    0 netromaster over 7 years ago in reply to mp2100

    Oh yes, based on his recommendations I would use a cheap nodemcu to read the pulse before sending it to the pi for more calculations. Or better still, I might just use the nodemcu for everything.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer