• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Raspberry Pi Forum How to connect a ADAFRUIT16x32 RGB LED Matrix Panel to a Raspberry Pi 4
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 7 answers
  • Subscribers 705 subscribers
  • Views 6134 views
  • Users 0 members are here
  • raspberry_pi
Related

How to connect a ADAFRUIT16x32 RGB LED Matrix Panel to a Raspberry Pi 4

harness68
harness68 over 7 years ago

I am having difficulty.  I assume I have connected the 16x32 RGB LED Matrix Panel to a Raspberry Pi 4 I have but It never displays.  I have followed all the tutorials on ADAFRUIT but they only confirm the pin out connection to a Pi3.  has anyone ever got this to work?

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 7 years ago

    Well I did more research and you cannot handle this on a Raspberry Pi as is:

     

    The GPIO pins are connected to the +3.3V rails. When used for input they are able to read voltages. When used for output they may be set to +3.3V (high) or 0V (low). There are 4 different types of GPIO pins on the Raspberry Pi.

    Because the Pi is 3.3V and the Adafruit 16x32 RGB LED Matrix Panel is 5 V, just connecting it would not work. But not all is lost. Look at https://www.sparkfun.com/products/12009  which convert both directions for this problem. Make sure to get enough for all the pins you will be using.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 7 years ago

    Well I did more research and you cannot handle this on a Raspberry Pi as is:

     

    The GPIO pins are connected to the +3.3V rails. When used for input they are able to read voltages. When used for output they may be set to +3.3V (high) or 0V (low). There are 4 different types of GPIO pins on the Raspberry Pi.

    Because the Pi is 3.3V and the Adafruit 16x32 RGB LED Matrix Panel is 5 V, just connecting it would not work. But not all is lost. Look at https://www.sparkfun.com/products/12009  which convert both directions for this problem. Make sure to get enough for all the pins you will be using.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • harness68
    0 harness68 over 7 years ago in reply to clem57

    Done, still got problems