• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Raspberry Pi Forum How to connect a ADAFRUIT16x32 RGB LED Matrix Panel to a Raspberry Pi 4
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 7 answers
  • Subscribers 705 subscribers
  • Views 6134 views
  • Users 0 members are here
  • raspberry_pi
Related

How to connect a ADAFRUIT16x32 RGB LED Matrix Panel to a Raspberry Pi 4

harness68
harness68 over 7 years ago

I am having difficulty.  I assume I have connected the 16x32 RGB LED Matrix Panel to a Raspberry Pi 4 I have but It never displays.  I have followed all the tutorials on ADAFRUIT but they only confirm the pin out connection to a Pi3.  has anyone ever got this to work?

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 7 years ago

    harness68  What software did you try? Do you have a digital meter to check the voltage changes to the panel? I have done simple LED's with no problem. My suggestion is check for the obvious before going too deep.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • harness68
    0 harness68 over 7 years ago in reply to clem57

    I did check the power and it was at 5 v  I think I need to double check the jumper connections to the 40 pin connector.  As for the software I used the suggested software (https://github.com/hzeller/rpi-rgb-led- ... es-api-use)

    It did give me a few issues at the command line

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 7 years ago in reply to harness68

    Good voltage of 5 V. It also suggested to supply around 2 amps externally and not from the Pi. Also in terms of software, the GPIO pins need to act as a PWM switch on and off at a frequency or duty cycle to make the LED's "glow". The faster the switching, the brighter the "glow". An Arduino has hardware and CPU dedicated to do this whereas the Raspberry Pi relies on software OS and is less deterministic.

     

    Keep in mind that these displays are designed to be driven by FPGAs or other high speed processors: they do not have built in PWM control of any kind. Instead, you're supposed to redraw the screen over and over to 'manually' PWM the whole thing. On a 16 MHz arduino, we managed to squeeze 12-bit color (4096 colors) with 20% CPU usage but this display would really shine if driven by any FPGA, CPLD, Propeller, XMOS or other high speed multi-core controller. The good news is that the display is pre-white balanced with nice uniformity so if you turn on all the LEDs its not a particularly tinted white.

    The above to me says the Raspberry Pi not very well suited although may be workable. If the Raspberry Pi gets busy CPU wise, the GPIO pins may not be driven at the desired rate due to interference. I have not examined the demo software to understand how it works.

     

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 7 years ago in reply to harness68

    Good voltage of 5 V. It also suggested to supply around 2 amps externally and not from the Pi. Also in terms of software, the GPIO pins need to act as a PWM switch on and off at a frequency or duty cycle to make the LED's "glow". The faster the switching, the brighter the "glow". An Arduino has hardware and CPU dedicated to do this whereas the Raspberry Pi relies on software OS and is less deterministic.

     

    Keep in mind that these displays are designed to be driven by FPGAs or other high speed processors: they do not have built in PWM control of any kind. Instead, you're supposed to redraw the screen over and over to 'manually' PWM the whole thing. On a 16 MHz arduino, we managed to squeeze 12-bit color (4096 colors) with 20% CPU usage but this display would really shine if driven by any FPGA, CPLD, Propeller, XMOS or other high speed multi-core controller. The good news is that the display is pre-white balanced with nice uniformity so if you turn on all the LEDs its not a particularly tinted white.

    The above to me says the Raspberry Pi not very well suited although may be workable. If the Raspberry Pi gets busy CPU wise, the GPIO pins may not be driven at the desired rate due to interference. I have not examined the demo software to understand how it works.

     

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer