• Products and Partners
    Products and Partners
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
Raspberry Pi
  • Products and Partners
  • More
Raspberry Pi
Raspberry Pi Forum How to connect a ADAFRUIT16x32 RGB LED Matrix Panel to a Raspberry Pi 4
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 7 answers
  • Subscribers 705 subscribers
  • Views 6134 views
  • Users 0 members are here
  • raspberry_pi
Related

How to connect a ADAFRUIT16x32 RGB LED Matrix Panel to a Raspberry Pi 4

harness68
harness68 over 7 years ago

I am having difficulty.  I assume I have connected the 16x32 RGB LED Matrix Panel to a Raspberry Pi 4 I have but It never displays.  I have followed all the tutorials on ADAFRUIT but they only confirm the pin out connection to a Pi3.  has anyone ever got this to work?

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 7 years ago

    As Clem says, it's very likely that the logic levels are incompatible. A lot of these 5V display boards use older logic ICs with non-3.3V-compatible inputs, and you'll either get nothing on the display, or stuff that looks like it sometimes works with corruption.

    There's also a high chance of power related issues, or software issues, if you're trying with a different version Pi. So, it's not surprising it isn't working. But, without photos showing your setup, including power source, and the output you got when installing and running the code (since you mention it did give you issues) it isn't possible to troubleshoot those aspects easily.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Problemchild
    0 Problemchild over 7 years ago in reply to shabaz

    Definitely  a 3.3-5v voltage level problem. I've not used their display but many others and they are all 5V using TTL shift registers for the most part and often CMOS so the 3.3v logic will be out of spec.

    Notice on the LED hat they use a separate 5V input and a 5V levelshifter. a bunch of transistors would do it as well up to you ...fortunately the levelshifting is all one way so easy enough!!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Problemchild
    0 Problemchild over 7 years ago in reply to shabaz

    Definitely  a 3.3-5v voltage level problem. I've not used their display but many others and they are all 5V using TTL shift registers for the most part and often CMOS so the 3.3v logic will be out of spec.

    Notice on the LED hat they use a separate 5V input and a 5V levelshifter. a bunch of transistors would do it as well up to you ...fortunately the levelshifting is all one way so easy enough!!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer