Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Writing threads into code for 4 channel relay on pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 26 replies
  • Answers 9 answers
  • Subscribers 707 subscribers
  • Views 6284 views
  • Users 0 members are here
  • rasberry_pi_3_b_plus
Related

Writing threads into code for 4 channel relay on pi

john2674
john2674 over 6 years ago

Hi i am a super noob at all things PI, i have done a few simple projects. That said coding is really new to me. Ive read python for dummies and quite a few articles on the web so far, but my latest project im stuck.

Im trying to write a code to controll a 4 channel relay board with my pi. But i want my relays to turn off and on at different intervals independant of each other. So far i think i need to use threading commands, but im not sure how to write them? As an example of what im trying to accomplish.

Relay 1 on 3 seconds off 5 seconds repeating forever

Relay 2 on 5 minutes then off permanently

Relay 3 on permanently

Relay 4 on permanently

 

If anybody can point me in a direction where i can learn these code commands i will be super grateful!

Ive tried searching all over and cant find what i need. Im sure i just need to get better at searching though lol.

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 6 years ago

    Hi John,

     

    The periodic counter/tick system recommended by Frank and Cris is a decent way to implement this.

    For what it's worth, here's some code just tried - it too uses a tick, in this case using some 'asyncio' library.

    This only works with very recent versions of Python though (Python 3.8, and perhaps Python 3.7).

     

    The beginning bit (lines 1-32) just sets up the framework for the ticks. Lines 33 onward handle the relay logic.

    There is a tick for 1 second, a tick for 10 seconds, and a tick for 60 seconds. I just used the 1 second and 60 second ticks.

     

    I'm a Python beginner (I don't like it much but slowly beginning to appreciate its usefulness) so I'm sure there are better ways to do it in Python, but this seemed to work. You'd need to replace or augment the lines containing print messages, to perform the actual relay switching.

    It outputs a dot every second, a D every 10 seconds, and an M every 60 seconds, and a relay-related message after 3, 8 seconds and 5 minutes.

     

    The program starts at line 67, because everything above it are functions.

     

    #!/usr/bin/python3.8
    import asyncio
    
    
    PERIOD = 1.0
    FOREVER = True
    counter=0
    
    
    # these three variables become 1 when 1, 10 or 60 seconds expire
    event1=0
    event10=0
    event60=0
    
    
    # counters for relays. rel1ctr counts in seconds, rel2ctr counts in minutes
    rel1ctr=0
    rel2ctr=0
    
    
    # tick routine. This updates the event variables
    async def tick():
      await asyncio.sleep(PERIOD)
      global counter, event1, event10, event60
      counter=counter+1
      if (counter%10==0):
        event10=1
      if (counter%60==0):
        event60=1
        counter=0
      event1=1
    
    
    # main function which checks the event variables and handles the relay states
    async def mainprog():
      global event1, event10, event60
      global rel1ctr, rel2ctr
      await asyncio.sleep(0.1)
    
    
      if (event1):
        event1=0
        print(".")
        rel1ctr=rel1ctr+1
        if (rel1ctr==3): # 3 seconds expired?
          print("relay 1 ON")
        if (rel1ctr>=8): # 3+5=8 seconds expired?
          print("relay 1 OFF")
          rel1ctr=0 # set back to zero so we can repeat the sequence for relay 1
    
    
      if (event10):
        event10=0
        print("D")
    
    
      if (event60):
        event60=0
        print("M")
        rel2ctr=rel2ctr+1
        if (rel2ctr>=5): # 5 minutes expired?
          print("relay 2 OFF")
    
    
    
    
    print("set relay 1 off")
    print("set relay 2 on")
    print ("set relay 3 on")
    print ("set relay 4 on")
    while FOREVER:
      asyncio.run(tick())
      asyncio.run(mainprog())

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • fmilburn
    0 fmilburn over 6 years ago in reply to shabaz

    Thanks for posting that Shabaz.  My experience with Python is limited and I am coming back to it after quite a bit of time away and am not familiar with the asyncio library.  Will check it out...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • fmilburn
    0 fmilburn over 6 years ago in reply to shabaz

    Thanks for posting that Shabaz.  My experience with Python is limited and I am coming back to it after quite a bit of time away and am not familiar with the asyncio library.  Will check it out...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 6 years ago in reply to fmilburn

    Hi Frank,

     

    Thanks! It is new to me too, not sure I like it or if I'm using it correctly, apparently it's the new way to do asynchronous stuff. Much of the documentation for it, perhaps because it is recent, expects a higher level of knowledge than I had..

    For simple stuff JavaScript has a 'setTimer' capability to create a type of tick function. It isn't pretty either, but at the end of the day we're trying to replicate a simple old-school timer interrupt type capability, rather than require a decent app framework so it's not so bad I guess..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer