Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Python help with GPIO
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 27 replies
  • Answers 10 answers
  • Subscribers 705 subscribers
  • Views 5265 views
  • Users 0 members are here
  • raspberry_pi
Related

Python help with GPIO

rcayot
rcayot over 6 years ago

Okay, I guess it is time to ask for help.  I have learned how to breadboard up a set of traffic lights, a button and a buzzer.  I can get them all to work with simple python programs.  Now I want to interrupt the normal light sequence when the button is pushed.  I can even get a detect event to work.  What I do not seem to be able to do is condition the "if" or "while" loop for the lights on the event. 

 

I have a callback and it seems to work, so I can print the status of the "button is pressed" but I cannot pass it as "true" to the loop.  I suspect it may be that when defining "btnpushed" it is local to only the callback loop?

 

i can self learn, but most of the tutorials I see are very single topic context, like what is a while loop or what is an if loop.  Any pointers to a good example of using these functions would be great!

 

i hope this is clear.

 

Roger Ayotte

  • Sign in to reply
  • Cancel
Parents
  • rcayot
    0 rcayot over 6 years ago

    okay, here is the code

     

    import RPi.GPIO as GPIO
    
    
    from time import sleep
    from signal import pause
    GPIO.setmode(GPIO.BCM)
    
    
    GPIO.setup(25, GPIO.OUT, initial=GPIO.LOW)  # red LED
    GPIO.setup(12, GPIO.OUT, initial=GPIO.LOW)  # yellow LED
    GPIO.setup(20, GPIO.OUT, initial=GPIO.LOW)  # green LED
    
    btnpushed = 0
    
    GPIO.setup(26, GPIO.IN, pull_up_down=GPIO.PUD_UP)
    def cb1(channel):
        btnpushed == 1
        print(btnpushed)
       
    GPIO.add_event_detect(26, GPIO.FALLING, callback=cb1, bouncetime=300)
    
    try:
        while btnpushed == 0:
            GPIO.output(20, GPIO.HIGH)  # green on
            sleep(5)  #
            GPIO.output(20, GPIO.LOW)  # green off
            sleep(0.01)
            GPIO.output(12, GPIO.HIGH)  # yellow on
            sleep(2)
            GPIO.output(12, GPIO.LOW)  # yellow off
            GPIO.output(25, GPIO.HIGH)  # red on
            sleep(5)
            GPIO.output(25, GPIO.LOW)  # red off
            pause
    
    
    except KeyboardInterrupt:
        GPIO.cleanup((25, 26, 12, 20))
    GPIO.cleanup((25, 26, 12, 20))

     

    what I am trying to do is use the boolean 1, or 0 for btnpushed to interrupt the light loop.  whenever I push the button, I get a zero printed.  and the light sequence keeps going.  Will try the 'not' later.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fmilburn
    0 fmilburn over 6 years ago in reply to rcayot

    Do you intend for line 17 to have == instead of =

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rcayot
    0 rcayot over 6 years ago in reply to fmilburn

    I happened to be trying that, it works when only = instead of ==

     

    I added a print statement after btnpushed = 0 and at the start of the program it prints 0, and when I press the button, it prints 1 but on every case the lights keep cycling.

     


    Roger

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rcayot
    0 rcayot over 6 years ago in reply to fmilburn

    I happened to be trying that, it works when only = instead of ==

     

    I added a print statement after btnpushed = 0 and at the start of the program it prints 0, and when I press the button, it prints 1 but on every case the lights keep cycling.

     


    Roger

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • easyejl
    0 easyejl over 6 years ago in reply to rcayot

    well, the single = is what is correct there, but then after that you still have to deal with the issue that the callback comes in on a separate thread from the main thread, and its only a 1 in the thread that is the callback, not in main.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to rcayot

    rcayot  wrote:

     

    I happened to be trying that, it works when only = instead of ==

     

    I added a print statement after btnpushed = 0 and at the start of the program it prints 0, and when I press the button, it prints 1 but on every case the lights keep cycling.

     


    Roger

     

    That's because every variable you're modifying in that def block is _local_. You need to define it as global.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rcayot
    0 rcayot over 6 years ago in reply to shabaz

    yes? using btnpushed as global worked as far as getting the loop interrupted?

     

    Now back to work on the rest of it!

     

    Thanks all who helped!

     

    Roger Ayotte

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • genebren
    0 genebren over 6 years ago in reply to rcayot

    Roger,

     

    I would assume that you will also need an GPIO.add_event_detect(26, GPIO.FALLING, callback=cb1, bouncetime=300) statement to detect GPIO.RISING to clear btnpushed in order to get your loop running again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 6 years ago in reply to shabaz

    Please read my post before...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rcayot
    0 rcayot over 6 years ago in reply to genebren

    Thanks, I was wondering how I was going to do that!

    roger