Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum can i use my laptop to program the Raspberry Pi with USB port or another way? what would i need  to do?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 7 answers
  • Subscribers 705 subscribers
  • Views 2524 views
  • Users 0 members are here
  • raspberry_pi
Related

can i use my laptop to program the Raspberry Pi with USB port or another way? what would i need  to do?

larrynewuser
larrynewuser over 6 years ago

can i use my laptop to program the Raspberry Pi with USB port or another way? what would i need  to do?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 6 years ago

    When you say "program" the Raspberry Pi, this could mean a lot of things.  Too vague for the folks who have responded.  Some possible guesses at what you mean:

    1. Write programs on the Raspberry Pi.
    2. Copy various data to the Raspberry Pi to be used there.

     

    Also, what O/S is your laptop running?  MacOS?  Linux/Unix?  Windows?

     

    You do not usually need a direct hardware connection to the RPi.  If both computers are sharing the same router (same LAN), then the simplest thing to do is connect to it with one of the IP protocols.  To do that, first find out the IP address of the RPi in one of two ways:

    (a) On the RPi with keyboard, mouse, and display, run `hostname -I` in a terminal window.  Standard output shows you the IP address.

    (b) Assuming (a) is not possible because the RPi is currently "headless", login to the router and figure out which connected client is the RPi.

     

    The following comments apply to laptops running MacOS, Linux, and Unix; Windows has equivalents.

     

    Once you have the IP address, assuming `ssh` services are enabled on the RPi, you can connect to it in a terminal window.  Suppose that the RPi is at 192.168.1.201.  Then, execute `ssh -X pi@192.168.1.201`.  The -X option allows you to run X-Windows programs at the RPi like `leafpad` or `gedit` for editing RPi local files with a GUI.

     

    Also, knowing the IP address of the RPi, you can copy files from the laptop to the RPi (or vice versa) using a network copy utility like `scp` or `rsync`.

     

    Please tell us some more of what you are trying to do.

     

    P.S. Take a look at this which might be helpful: Accessing and Controlling the Pi

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 6 years ago

    When you say "program" the Raspberry Pi, this could mean a lot of things.  Too vague for the folks who have responded.  Some possible guesses at what you mean:

    1. Write programs on the Raspberry Pi.
    2. Copy various data to the Raspberry Pi to be used there.

     

    Also, what O/S is your laptop running?  MacOS?  Linux/Unix?  Windows?

     

    You do not usually need a direct hardware connection to the RPi.  If both computers are sharing the same router (same LAN), then the simplest thing to do is connect to it with one of the IP protocols.  To do that, first find out the IP address of the RPi in one of two ways:

    (a) On the RPi with keyboard, mouse, and display, run `hostname -I` in a terminal window.  Standard output shows you the IP address.

    (b) Assuming (a) is not possible because the RPi is currently "headless", login to the router and figure out which connected client is the RPi.

     

    The following comments apply to laptops running MacOS, Linux, and Unix; Windows has equivalents.

     

    Once you have the IP address, assuming `ssh` services are enabled on the RPi, you can connect to it in a terminal window.  Suppose that the RPi is at 192.168.1.201.  Then, execute `ssh -X pi@192.168.1.201`.  The -X option allows you to run X-Windows programs at the RPi like `leafpad` or `gedit` for editing RPi local files with a GUI.

     

    Also, knowing the IP address of the RPi, you can copy files from the laptop to the RPi (or vice versa) using a network copy utility like `scp` or `rsync`.

     

    Please tell us some more of what you are trying to do.

     

    P.S. Take a look at this which might be helpful: Accessing and Controlling the Pi

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • colporteur
    0 colporteur over 6 years ago in reply to e14 Contributor

    Your response mirrors my own conundrum from the members question. The word programming could have a number of connotations given the diversity of members in this community. I'm stingy with the time I take to respond. Unless I am crystal clear on the requirements or the dialog is to flush out the requirements, I try not to make suggestion.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer