Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Help: Encountering CAN Bus Problem on SmartEdge IIoT Gateway
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 27 replies
  • Answers 17 answers
  • Subscribers 704 subscribers
  • Views 7607 views
  • Users 0 members are here
  • raspberry_pi
  • raspberrypi
  • smartedge iiot gateway
  • canbus
Related

Help: Encountering CAN Bus Problem on SmartEdge IIoT Gateway

khz_321
khz_321 over 6 years ago

Hi All,

 

I was wondering if anyone has had any experience using the CAN Controller on the SmartEdge IoT Gateway

The box has a Built-in MCP2515 CAN Controller on board, which is great & why I selected it for a project that requires CAN

 

For the most part, it works fine, but every so often I'm encountering "Garbage" data coming from the chipset (at a rate of about 1 message every 10 mins with a message cycle of 100ms)

This is shown below, when simply monitoring using candump and nothing else

 

image

the shown 67 EB in bytes 7 & 8 are the bits Garbage Data in question. It should be noted that when I do get the garbage, its always the same 2 Bytes and same values.

 

The sender device is broadcasting the same message repeatedly, so there should be no changes at all!

 

I was also able to confirm that it is not present on the physical bus by using a PCAN USB and datalogging with Pcan-View at the same time.

The data dump from Pcan-View shows no messages like the one highlighted!

 

Seems like this is happening on the Controller Hardware or Driver Implementation side on the IIoT Gateway

Anyone encountered this before? Either on this product or any other Raspberry Pi ?

 

I've tried adjusting the bit timing, sampling point, everything I could think of, but still encountering a random error every so often

 

Here is my CAN settings from /etc/network/interfaces

 

auto can0
iface can0 inet manual
   pre-up /sbin/ip link set can0 type can bitrate 250000 sample-point 0.875 triple-sampling on
   up /sbin/ifconfig can0 up
   down /sbin/ifconfig can0 down

 

And here is the output of ip -details -statistics link show can0

ip -details -statistics link show can0
4: can0: <NOARP,UP,LOWER_UP,ECHO> mtu 16 qdisc pfifo_fast state UNKNOWN mode DEFAULT group default qlen 10
    link/can  promiscuity 0 
    can <TRIPLE-SAMPLING> state ERROR-ACTIVE restart-ms 0 
  bitrate 250000 sample-point 0.875 
  tq 250 prop-seg 6 phase-seg1 7 phase-seg2 2 sjw 1
  mcp251x: tseg1 3..16 tseg2 2..8 sjw 1..4 brp 1..64 brp-inc 1
  clock 8000000
  re-started bus-errors arbit-lost error-warn error-pass bus-off
  0          0          0          0          0          0         numtxqueues 1 numrxqueues 1 gso_max_size 65536 gso_max_segs 65535 
    RX: bytes  packets  errors  dropped overrun mcast   
    17224264   2153033  0       1508    0       0       
    TX: bytes  packets  errors  dropped carrier collsns 
    16         2        0       0       0       0

 

Note: Kernel Version 4.14.79-v7+, & Software Image: avnet_iot_demo_20190719a_shrink

(Also tried with latest release avtse-iiotg-v-11-20200326.img, which apparently updated the MCP2515 driver, but problem still persists)

 

Any advice? 

  • Sign in to reply
  • Cancel
Parents
  • Jan Cumps
    0 Jan Cumps over 5 years ago

    I have never seen this happen.

    I have a smartedge on my desk here, attached to a single CAN device. I haven't seen bogus traffic at Linux level.

    I'll leave it running tonight with candump active. Let's see if I received something unexpected.

    I'm using image avnet_iot_demo_20190719a_shrink.

     

    Config:

    auto can0
    iface can0 inet manual
       pre-up /sbin/ip link set can0 type can bitrate 500000
       up /sbin/ifconfig can0 up
       down /sbin/ifconfig can0 down

     

     

    Log (rebooted to have a clean test start point):

    avnet@smartedge:~ $ ip -details -statistics link show can0
    4: can0: <NOARP,UP,LOWER_UP,ECHO> mtu 16 qdisc pfifo_fast state UNKNOWN mode DEFAULT group default qlen 10
        link/can  promiscuity 0
        can state ERROR-ACTIVE restart-ms 0
              bitrate 500000 sample-point 0.875
              tq 125 prop-seg 6 phase-seg1 7 phase-seg2 2 sjw 1
              mcp251x: tseg1 3..16 tseg2 2..8 sjw 1..4 brp 1..64 brp-inc 1
              clock 8000000
              re-started bus-errors arbit-lost error-warn error-pass bus-off
              0          0          0          0          0          0         numtxqueues 1 numrxqueues 1 gso_max_size 65536 gso_max_segs 65535
        RX: bytes  packets  errors  dropped overrun mcast
        0          0        0       0       0       0
        TX: bytes  packets  errors  dropped carrier collsns
        0          0        0       0       0       0

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 5 years ago in reply to Jan Cumps

    I didn't get any bogus traffic with a working circuit.

    I deliberately sent one command on the bus after 12 hours waiting, and it was reported by  candump.

    Nothing else happened during the 12 hours.

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • roryyorke
    0 roryyorke over 5 years ago in reply to michaelkellett

    The kernel module unload-load workaround didn't help.

     

    We have found something interesting; when a packet is corrupted, the final two bytes are a bit-shuffled variant of the packet arbitration ID.

     

    Specifically, the last two bytes become, interpreted as a little-endian number,  `(arbitration_id & 0x7) << 13) + (arbitration_id >> 3)`

     

    We're using 12-bit arbitration IDs; I don't know if there's similar determinism with extended IDs.

     

    We've verified the above with simple Python 3 scripts; I don't see an "attach" option here, but I'm happy to mail the code to anyone who wants it.  You will need two SmartEdges to use these scripts "as-is".

     

    Latest result I have from running these scripts is, of 1401502 packets received, 1888 were bad, and all 1888 bad packets match the bit-shuffle pattern above.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 5 years ago in reply to roryyorke

    roryyorke  wrote:

    ... I don't see an "attach" option here, but I'm happy to mail the code to anyone who wants it.  You will need two SmartEdges to use these scripts "as-is"...

     

    You can't attach code to comments or to someone else's post. You can upload them to gist.github.com, and link here.

     

    I have 2 SmartEdges and should be able to replicate the test.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • roryyorke
    0 roryyorke over 5 years ago in reply to Jan Cumps

    I've put the code at https://github.com/roryatario/smartedge-can-tester

     

    The scripts need the python3-can package ("apt install ...").

     

    Run "python3 sendsimple.py" on one SmartEdge, and "python3 recvsimple.py" on the other; recvsimple will print number of total, bad, and bad-matching-pattern packets once a second.

     

    You might need to increase the transmit queue on the sender (`ip link set can0 txqueuelen 50`).

     

    FWIW, I've just confirmed that I see this bug in a candump recording from packets sent from a completely different device, so the error occurs on the receiving side.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 5 years ago in reply to roryyorke

    I've done the hardware setup.

    image

     

    The MicroChip analyzer only snoops traffic. It doesn't interfere.

    I'll now install the Python libs and check the test scripts.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 5 years ago in reply to Jan Cumps

    Lucky you have all the right gear to replicate the problem.

     

    Good hunting.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 5 years ago in reply to Jan Cumps

    Enabled the interface on both - tested with and without changing the txqueuelen:

     

    sudo ip link set can0 up type can bitrate 125000

    sudo ifconfig can0 up

    sudo ip link set can0 txqueuelen 50

     

    Then first box send, 2nd box receive

     

    python3 sendsimple.py

    python3 recvsimple.py

     

     

    without tx queue change

    image

     

    with buffer length 50:

    image

     

    The CAN analyzer does not detect any traffic errors. The data on the bus seems OK.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 5 years ago in reply to michaelkellett

    michaelkellett  wrote:

     

    ... I had a quick look at the MCP251x driver.

    Interesting - not the kind of code you would expect to find in a car or plane.

     

    eg:

     

    do {

            mdelay(MCP251X_OST_DELAY_MS);

            reg = mcp251x_read_reg(spi, CANSTAT);

        } while (!reg && retries--);

     

    I haven't got time now but I'll run that loop through PCLint and see how many whinges it gives.

     

    That's not in the original Linux code for this CAN driver. I see that this is a change that Avnet made to the code base.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • phoenixcomm
    0 phoenixcomm over 5 years ago in reply to Jan Cumps

    Jan Cumps michaelkellett That loop is evil. why is it introducing the mdelay()?? I have most of my own code base runs on interrupts!

    ~~Cris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • roryyorke
    0 roryyorke over 5 years ago in reply to Jan Cumps

    Thanks for repeating the test.

     

    The txqueuelen is only be needed if, on the sender side,  you get "buffer full" errors; I may have used it when I didn't have the `time.sleep(0.0001)` call in the sender loop.

     

    In your first run (txqueuelen=0) we can see a replication the behaviour I described: there's one bad packet (at 1595 packets), and, from the second "1" on that line, it matches the corruption pattern.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 5 years ago in reply to roryyorke

    You could log an issue in github, on the repository where the CAN code sits.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 5 years ago in reply to roryyorke

    You could log an issue in github, on the repository where the CAN code sits.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer