Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Could anyone help me out with  the Raspi Zero and BMP085?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 3 answers
  • Subscribers 704 subscribers
  • Views 3108 views
  • Users 0 members are here
  • rasberry pi
  • rasberry pi zero
  • raspberry_pi
  • bmp085
  • assistance
Related

Could anyone help me out with  the Raspi Zero and BMP085?

cagan
cagan over 5 years ago

Hello! I've been working with a Rasberry Pi zero for the past couple weeks, following a tutorial to interface with a Barometer sensor (the BMP 085,) and I've ran into a bit of a snag.
The sensor works, everything works electrically, I'm sure, that's more my background, but I'm not sure the code is set up right, or if the Pi can even tell something is connected.
When I try to run a sample code provided with files I didn't get from the tutorial (I found them on Adafruit's site) I get the following error:

Traceback (most recent call last):

File "simpletest.py", line 48, in <module>

print('Temp = {0:0.2f} *C'.format(sensor.read_temperature()))

File "build.bdist.linux-armv6l/egg/Adafruit_BMP/BMPO85.py", line 143, in read_

temperature

ZeroDivisionError: integer division or modulo by zero


I don't know any Python, just Java, so any help with interpreting this stuff and possibly fixing it would be wonderful, I'll leave links to Imgur images of my setup, with the third images containing my issue.

Here's a link to the tutorial:
https://tutorials-raspberrypi.com/raspberry-pi-and-i2c-air-pressure-sensor-bmp180/

https://imgur.com/mg8mWpx

This is the sensor.

https://imgur.com/YoDkQlo
This is the wiring setup, the blue wire on the top right will be replaced later, I just haven't had the chance to solder more pins onto the holes.

https://imgur.com/kctV6RP
This is me attempting to run a sample code provided to me from the tutorial, with the errors in question.



  • Sign in to reply
  • Cancel
Parents
  • javagoza
    0 javagoza over 5 years ago

    Hi, David,

     

    From the photo it seems to be a BMP388 Barometric Pressure Sensor not a BMP 085

    Use another library like https://github.com/adafruit/Adafruit_CircuitPython_BMP3XX

     

     

    BMP388 Barometric Pressure Sensor - CQRobot-Wiki

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • cagan
    0 cagan over 5 years ago in reply to javagoza

    Alright, I'll try this!
    Also, to reply to Shabaz, yes, that's a ground connection. The sensor did not appear to be getting power before I made that connection, I don't have anymore pins I can solder to the board, it's temporary until I can rectify that.
    I've used the i2c detection before, and it did indeed find something.
    I got a large array of numbers on the terminal window, which the tutorial I was following said was correct, is that not so?



    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 5 years ago in reply to cagan

    Hi David,

     

    If it's the wrong chip (as Enrique mentions) then that code will not work in any case. The code needs to be compatible with the chip in question.

    Poking the jumper wire into the hole and relying on natural wire springiness might work but more than likely is not going to be an adequate connection for a stream of data, it's not a case of maintaining electrical connectivity briefly, it needs to be sustained. If it isn't, then the software may crash or give an error, because even a few nanoseconds of disconnection can destroy the communication if it's at a critical moment. There are no reattempts in most simple demo code, the code will likely generate an error or silently output garbage or crash.

    One option is to solder a wire into the hole temporarily so that you have a stable connection, and then desolder and add the connector at a later date. Anyway, the code and chip compatibility needs to be checked. Normally you can refer to the datasheet of the chip to see the specifics, to see if it has identical communication (unlikely - most chips have different communication schemes). Sometimes the i2cdetect command can be used to narrow down what chip you have, but wherever you ordered it from should have that detail if it's not written on the board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 5 years ago in reply to cagan

    Hi David,

     

    If it's the wrong chip (as Enrique mentions) then that code will not work in any case. The code needs to be compatible with the chip in question.

    Poking the jumper wire into the hole and relying on natural wire springiness might work but more than likely is not going to be an adequate connection for a stream of data, it's not a case of maintaining electrical connectivity briefly, it needs to be sustained. If it isn't, then the software may crash or give an error, because even a few nanoseconds of disconnection can destroy the communication if it's at a critical moment. There are no reattempts in most simple demo code, the code will likely generate an error or silently output garbage or crash.

    One option is to solder a wire into the hole temporarily so that you have a stable connection, and then desolder and add the connector at a later date. Anyway, the code and chip compatibility needs to be checked. Normally you can refer to the datasheet of the chip to see the specifics, to see if it has identical communication (unlikely - most chips have different communication schemes). Sometimes the i2cdetect command can be used to narrow down what chip you have, but wherever you ordered it from should have that detail if it's not written on the board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • cagan
    0 cagan over 5 years ago in reply to shabaz

    I soldered it before trying that new library that Enrigue sent me, the git page said it came with example code, but I can't find, I'm certain I've installed the library as it's right where the BMP085 library is when I installed it.
    I'll show it here: