Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi Splashscreen issue
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 707 subscribers
  • Views 1453 views
  • Users 0 members are here
  • raspberry_boot_issues
  • raspberrypi
Related

Raspberry Pi Splashscreen issue

e14 Contributor
e14 Contributor over 12 years ago

Hi - I got a Raspberry Pi a while ago now, and whenever I booted it with the "Raspbian Wheezy" Image, it would boot up fine. But, after shutdown/restart, when the Pi attempts to turn back on, my Pi freezes on the coloured RGB splash screen most people see when they boot their Pi. This means I can not restart the device automatically, but have to unplug power, and wait up to 2 minutes "cooldown" before booting my Pi, in which case it works. I'd always assumed this was a bug with my Kernel Image, but after reinstalling/re downloading/re writing etc. I find I still have the same problem! I have switched to NOOBS, which still presents the same issue. Is this an issue with a component like an SD card not being read properly, or in fact there is a problem with the Pi? Again, this happened when I first got the Pi, so should I also be entitled to a new Pi if it is the fault of Element14?

 

Thanks, Yaseen.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I have had a similar issue, which might be worthy to try this solution.

     

    My rPi, last year would not reboot properly.  I had purchased multiple Pi's so I was fortunate to be able to cross-check the issue; swap cards and hardware.

     

    For this particular issue, it was the SD card that was a problem.  A card which I already had in my bucket of spare parts, which worked for a few days until this occurred.  The other cards I had verified with the compatibility list before purchasing new cards.  All those worked with no problems.  This one was a 2gb card from a dead camera.  Not listed in the compat chart, and possibly did not work well with the Pi.

     

    The problem followed the card when changing the Pi it was inserted into.  Thus I made that assumption.  Rebuild the SD on a different card, and the problem went away, never returned.  Using the questionable 2gb card again, built a new image on it, and again I had another problem, this time would not boot due to a failure in the partition table.  That card is now back in the spare part bucket.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Thanks for the reply - I have bought an SD card directly from SanDisk, thinking my current SD card was probably a counterfeit, and yeah... I have not yet tested it though. But I have high hopes for it to work image.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Thanks for the reply - I have bought an SD card directly from SanDisk, thinking my current SD card was probably a counterfeit, and yeah... I have not yet tested it though. But I have high hopes for it to work image.