Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum pci bus on raspberry pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 16 replies
  • Answers 1 answer
  • Subscribers 709 subscribers
  • Views 2965 views
  • Users 0 members are here
  • pci
  • bus
  • raspberry_pi
  • pcie
Related

pci bus on raspberry pi

e14 Contributor
e14 Contributor over 12 years ago

Hello,

 

Is that possible to add a PCI or PCIe Bus on Raspberry pi?

 

If yes, how can i do it and what i need to buy?

 

King Regards,

Ricardo Silva

  • Sign in to reply
  • Cancel
Parents
  • gregoryfenton
    0 gregoryfenton over 12 years ago

    This just appeared in my mailbox:

     

    The 86Duino Zero Runs Linux on x86 - ELEKTOR.com | Electronics: Microcontrollers Embedded Audio Digital Analogue Test Me…

     

    It is an x86 based Arduino type board with PCI express built in. Hope it helps, I am looking at getting one image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • gregoryfenton
    0 gregoryfenton over 12 years ago

    This just appeared in my mailbox:

     

    The 86Duino Zero Runs Linux on x86 - ELEKTOR.com | Electronics: Microcontrollers Embedded Audio Digital Analogue Test Me…

     

    It is an x86 based Arduino type board with PCI express built in. Hope it helps, I am looking at getting one image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to gregoryfenton

    I can't help but think that a 300MHz x86 processor is going to feel horribly slow even compared to a Raspberry Pi.  Depends what you use it for I suppose.  I have a Minnowboard, 1GHz Intel Atom cpu, and it struggles with things the Pi doesn't. That 86Duino is a full 700MHz slower.

     

    PCIe appearing on lower end boards is welcome of course, but I'd be left wondering what PCIe card I could connect that the board wouldn't struggle to handle.  The choices it opens is the main point I suppose as other boards won't have those options.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to gregoryfenton

    This is not the piece that i try to find.

    I try to find a PCI BUS (female) not a PCI Card (male).

    Thanks anyway image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    The MinnowBoards are so expensive! Instead you can buy an Intel D2700 or something with Atom (NM10) processor.


    Basically i try to find an raspberry pi with PCI or PCIe. That would be perfect. As I can see it is impossible to find it.

     

    Thank you all image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Ricardo Silva wrote:

     

    This is not the piece that i try to find.

    I try to find a PCI BUS (female) not a PCI Card (male).

    If you look at the SoC they're using, it has both PCIe target (i.e. it acts as a pcie card) and Control (can control other PCIe cards) interfaces. You'd have to do some research on how it's wired up, what drivers etc, but it's possible that all you need is a simple mechanical adapter in order to be able to connect it to a card. Not a lot of details on their website though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I am looking for exactly the same thing. - And for almost the same reason you are!

     

    Have you had any success?