Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum pci bus on raspberry pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 16 replies
  • Answers 1 answer
  • Subscribers 709 subscribers
  • Views 2965 views
  • Users 0 members are here
  • pci
  • bus
  • raspberry_pi
  • pcie
Related

pci bus on raspberry pi

e14 Contributor
e14 Contributor over 12 years ago

Hello,

 

Is that possible to add a PCI or PCIe Bus on Raspberry pi?

 

If yes, how can i do it and what i need to buy?

 

King Regards,

Ricardo Silva

  • Sign in to reply
  • Cancel
Parents
  • gregoryfenton
    0 gregoryfenton over 12 years ago

    This just appeared in my mailbox:

     

    The 86Duino Zero Runs Linux on x86 - ELEKTOR.com | Electronics: Microcontrollers Embedded Audio Digital Analogue Test Me…

     

    It is an x86 based Arduino type board with PCI express built in. Hope it helps, I am looking at getting one image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to gregoryfenton

    I can't help but think that a 300MHz x86 processor is going to feel horribly slow even compared to a Raspberry Pi.  Depends what you use it for I suppose.  I have a Minnowboard, 1GHz Intel Atom cpu, and it struggles with things the Pi doesn't. That 86Duino is a full 700MHz slower.

     

    PCIe appearing on lower end boards is welcome of course, but I'd be left wondering what PCIe card I could connect that the board wouldn't struggle to handle.  The choices it opens is the main point I suppose as other boards won't have those options.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    The MinnowBoards are so expensive! Instead you can buy an Intel D2700 or something with Atom (NM10) processor.


    Basically i try to find an raspberry pi with PCI or PCIe. That would be perfect. As I can see it is impossible to find it.

     

    Thank you all image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    The MinnowBoards are so expensive! Instead you can buy an Intel D2700 or something with Atom (NM10) processor.


    Basically i try to find an raspberry pi with PCI or PCIe. That would be perfect. As I can see it is impossible to find it.

     

    Thank you all image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I am looking for exactly the same thing. - And for almost the same reason you are!

     

    Have you had any success?